STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F407 SPI Datasize and FSMC #WR operation DOUBLEs

Hi Team,​Basing on the lastest "STM32F4xx_StdPeriph_Driver" to Read SPI data and then write into external FSMC(8bit) device in the PWM interrupt like following .​//--------------------------------------------------------------------------------------...

0693W000006HzfNQAS.jpg
jhl14 by Associate II
  • 1377 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F439ZI + Eth + LwIP; no ping response

Hello,i have a Nucleo-144 board, where i replaced the STM32F429ZI for a STM32F439ZI.I used CubeMX 5.2.0 to create a ethernet test project just to ping the board and go further from there, but i cant get it to work.Ethernet is enabledEthernet interrup...

0690X000008B5dmQAC.png 0690X000008B5euQAC.png 0690X000008B5f4QAC.png 0690X000008B5fOQAS.png

Resolved! STM32F103 Custom HID; I'm stuck

Hi all,I'm Pierre, I am new to this community!I have found many great tips for some of my problems, but I moved into custom HID and I'm stuck.So here's what I am trying to do. I have two slave cards sending I2C data to the master. This is working gre...

Ple b.11 by Associate
  • 1109 Views
  • 1 replies
  • 0 kudos

STM32H7 Change USB buffers

I recently changed my SPI, I2C and USB HID to DMA. I changed buffers so they are in specific RAM sections which are accessible to DMA (RAM_D3 for I2C and RAM_D2 for SPI and USB). I am using DTCM RAM for stack, heap, data, etc. It was easy to change p...

USB type B on H7 (SOLVED)

Hi!I was thinking of building some sort of motherboard that can house a WaveShare Core H7xx STM32H7 board (so that I can connect peripherals using screw terminals). For USB communication I would use a USB type B, but I'm not sure how to connect the V...

0693W000006HFJgQAO.png