STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 missing USB device after DFU bootload

Hi,I have a bug with my bootload application on STM32H743ZI (my device is powered and bootloaded throw the same USB port)1 - I send a HID USB message to tell the micro to jump to bootloader2 - I bootload using DfuSe dll (it appears to work fine)3 - A...

Resolved! USB Device Custom HID Device cannot start on win10

Hi ST,I follow this video to implement my USB HID Project https://www.youtube.com/watch?v=3JGRt3BFYrM&ab_channel=STMicroelectronicsOn the Win7, it work perfect, but when I use Win10 as PC Host, it cannot workjust like bellow picture    Please Help ...

0693W000007CcmeQAC.png 0693W000007CcmjQAC.png 0693W000007CcmoQAC.png 0693W000007CcmtQAC.png
TWu.5 by Associate II
  • 3391 Views
  • 2 replies
  • 0 kudos

Resolved! Could TCPP01-M12 be used without the N-MOSFET?

We have a wide-input power management ic with buck-boost converter. 28V VBUS is not a problem. So is it possible to eliminate the N-MOSFET (at least in Sink mode)? If it is OK, what is your recommendation for connections of IN_GD, Gate, and Source pi...

matianfu by Associate II
  • 1203 Views
  • 1 replies
  • 1 kudos

TCP port number reused

I am using STM32 TCP Echo server client Cube IDE example. I have server and client device. I can connect first time successfully but when I reset the client, I get after 70 line in wireshark screenshot. How Can I solve this problem ? What is the reas...

DCtech by Associate II
  • 819 Views
  • 1 replies
  • 0 kudos

Over-current indication on USB host on STM32F2xx

Hello, I am using the STM32F2xx ev board to develop a simple application that utilizes the USB port as a HOST. I would like to check if a device has been connected to the port and it causes over-current on the USB.Looking into the source code, It see...

DZado.2 by Associate II
  • 1264 Views
  • 1 replies
  • 0 kudos