STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L152RE application shifted to new address results in hardfault FORCED on startup with debugger

I'm trying to implement a bootloader for my application and need to shift my application to a higher address. I've updated the linker script such that the application starts at address 0x08040200 and this seems to work. However, when I start debuggin...

Resolved! Usb stick Reading..

Hi guys.. I am trying to read the usb stick with STM32F746... I am always stucked becasue it doesn't read anything... Can you please help me ? Thanks a lot

SGasp.1 by Senior
  • 3456 Views
  • 1 replies
  • 0 kudos

eMMC on STM32H743 always Disk Error

Hi, Like old topic says : https://community.st.com/s/question/0D50X0000BbNEpXSQW/fatfs-emmc-always-frdiskerror?t=1573783271738 I`m trying to build project for STM32H743 with STM32CubeMX, and use eMMC for my storage space.​eMMC : Micron 4GBManager Fil...

0690X00000As3uPQAR.png

Which MCU should be suitable using Cloud?

Hi, everyone.I have a worry about choosing MCU.Well...my conditions are those.First, I would like to use 2 of Ethernet Ports.And then, I prefer to make cloud database system with X-cube if I would.I am also finding MCU through 'mcu finder', but It's ...

EHa.1 by Associate II
  • 1115 Views
  • 1 replies
  • 0 kudos

stm32L072cz PDM to PCM

Hi, I have stm32l072cz and I need to connect a digital microphone and make a sound level meter. There are no questions with the connection microphone, but there was a problem with the conversion of PDM to PCM. As I understand the library AudioPDM-MW ...

Vandr.1 by Associate II
  • 1089 Views
  • 0 replies
  • 0 kudos

Resolved! STM32H7 Dual Core DFU

I'm working with the STM32F7 dual-core capability for the first time. Using NUCLEO-H745ZI-Q, DfuSe Demo v3.0.6, DFU File Manager v3.0.6I have one program for the CM7 core and another for the CM4 core. I can enter the system bootloader by applying 3...

SEast.1 by Associate
  • 2300 Views
  • 2 replies
  • 0 kudos