STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F769 ethernet chip power up issue

Hello,This is nur. I need your help. I am working on STM32F769 phy chip , RMII interface. Once I apply power the stm chip then Ethernet cable clicked , there is no connection. if Ethernet cable does not click into place before power is applied to the...

nur by Associate II
  • 1499 Views
  • 2 replies
  • 0 kudos

Corrupted ETH Rx Buffer in STM32H7

Hello everyone,I'm running a webserver on a STM32H7. Code was generated with CubeIDE 1.5.0, using LwIP V2.1.2 and the Firmware-Package V1.8.0. So far, I had no problems receiving or transmitting smaller files, in the x-xx kB range from the MCU to a c...

_legacyfs_online_stmicro_images_0693W00000BaNHa.png _legacyfs_online_stmicro_images_0693W00000BaNGm.png _legacyfs_online_stmicro_images_0693W00000BaNMH.png _legacyfs_online_stmicro_images_0693W00000BaNOl.png
DWeb_2 by Associate III
  • 4069 Views
  • 5 replies
  • 0 kudos

P-L496_Cell02 can't find SIM

There are eSIM and Mirco_SIM in the Modem board, but it keep report: CST_modem_sim_init : Can't find sim on current slot. Increment sim slot.    CST_modem_sim_init : No more sim slot, no SIM found. Retry...     Any suggestion?

[STM32F769I-EVAL] Can I use both the Audio and Ethernet functionalities at the same time on an application?

So this question arises because the jumpers 3 and 6 of the board switch between either Audio or Ethernet, and I'm not sure in what capacity they're mutually exclusive or not.As an example imagine an application for audio streaming over Ethernet:can I...

Rrges.1 by Associate II
  • 2406 Views
  • 3 replies
  • 0 kudos

Hello Experts Could anyone suggest me how to convert the raw PCM values received in log file be to mp3 or .wav formats .And if there any libraries that could be included or any method? after conversion storing that into sdmmc and play that as loopback?

The Acquired PDM signal is from VM3000 mic and PDM2PCM conversion using stm32f745?could the acquired values be played as loopback to verify whether the acquired sound is in audible frequency to human ears? How could this be validated? all suggestions...

SG.4 by Associate II
  • 957 Views
  • 0 replies
  • 0 kudos

lwIP PPP protocol

Hi,How are you all doing?To our application we integrated ST cellular stack to work with QUECTEL Modem M66 and all required features are working expected.Now we decided to integrate lwIP stack from ST and use PPP protocol.I made the initial settings ...

ANaga.2 by Associate II
  • 3109 Views
  • 1 replies
  • 0 kudos

Resolved! HAL I2C Slave using DMA and interrupts. Has anyone found a good description of how to use the HAL DMA functions?

I see there are sequencing functions, but have found no examples or documentation on how to use them. I need to be able to RX an address, then a pointer, and then either read or write data on a restart, multiple bytes, then a stop.By sequencing funct...

JTayl.4 by Associate
  • 4826 Views
  • 2 replies
  • 0 kudos