2020-04-01 4:05 AM
Hi! I am trying to set ADC pre-scaler of my STM32G431KB however no matter what I do it never changes from 0x0.
I can setup ADC1 register without a problem but when it comes to ADC12_Common register nothing seems to be configurable.
Below there is my ADC configuration code.
//-------------ADC Configuration-------------//
ADC1->CR &= ~(ADC_CR_ADEN); //Disable ADC
ADC12_COMMON->CCR |= (0b00<<ADC_CCR_CKMODE_Pos); //Select ADC clock Source in Peripheral
ADC12_COMMON->CCR |= (0b1000<<ADC_CCR_PRESC_Pos); //ADC Clock divided by 32
ADC1->CR &= ~(ADC_CR_DEEPPWD); //Disable ADC Deep-Power-Down mode
ADC1->CR |= ADC_CR_ADVREGEN; //Enable ADC Voltage Regulator
DummyDelay(10000); //Delay for ADC Voltage regulator settling
ADC1->CFGR |= ADC_CFGR_CONT; //ADC continuous mode
ADC1->CFGR &= ~(ADC_CFGR_RES); //12-bit ADC
ADC1->SQR1 |= (0b0000 << ADC_SQR1_L_Pos) | (1 << ADC_SQR1_SQ1_Pos); // Only 1 conversion for ADC channel 1
ADC1->DIFSEL &= ~(ADC_DIFSEL_DIFSEL_0); //Single Ended Input
ADC1->CFGR2 |= (0b0001 << ADC_CFGR2_OVSS_Pos); //Over-sampling mode 1 bit shift
ADC1->CFGR2 |= (0b001 << ADC_CFGR2_OVSR_Pos); //Over-sampling ratio x4
ADC1->CFGR2 |= ADC_CFGR2_ROVSE; //Enable Over-sampling
ADC1->CFGR |= ADC_CFGR_DMAEN | ADC_CFGR_DMACFG; //Enable DMA for ADC and DMA in Circular Mode
ADC1->CR &= ~(ADC_CR_ADCALDIF); //Single Ended Mode Calibration
ADC1->CR |= ADC_CR_ADCAL; //Start Calibration
while(ADC1->CR & ADC_CR_ADCAL); //Wait Until Calibration Complete
ADC1->ISR |= ADC_ISR_ADRDY; //Clear ADRDY Flag
ADC1->CR |= ADC_CR_ADEN; //Enable ADC
while(!(ADC1->ISR & ADC_ISR_ADRDY)); //Wait Until ADC EnablesCan someone tell me what I am doing wrong in line 3 and 4 of above code?
2020-04-01 6:00 AM
Hello,
Beware the .svd file for the STM32G4 has the wrong address for ADC12_Common (and ADC5). If you're trying to read/write them from a debugger, it will reference to the wrong address. I've mentioned this previously, but ST has not updated...
Good luck!
Regards,
Dave
2020-04-01 6:20 AM
Thank you! You are right.
2020-04-01 7:23 AM
ADC12_COMMON->CCR |= (0b00<<ADC_CCR_CKMODE_Pos); //Select ADC clock Source in Peripheral
ADC12_COMMON->CCR |= (0b1000<<ADC_CCR_PRESC_Pos); //ADC Clock divided by 32
So these lines are correct right? The only issue is that I cannot see it in debugger right?
2020-04-15 12:47 PM
Hello,
Thank you for highlighting this.
Please find attached the new svd file for STM32G431 with the fix.
<name>ADC12_Common</name>
<description>Analog-to-Digital Converter</description>
<groupName>ADC</groupName>
<baseAddress>0x50000300</baseAddress> The correction (for all the G4 devices) is implemented internally and will be available in the ST web page.
Best Regards,
Imen
2020-09-09 12:01 PM
Hi!,
I think the STM32F303 has the same problem.
2020-09-09 12:26 PM
I don't know what debugger are you using, but you should be able to observe content on absolute addresses.
JW