STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interfacing with MEMS digital microphone

Hello,I'm using an stm32l151re to interface with mp34dt05-a mems microphone. I'm using it to determine noise level. The communication between smt32 mcu and the sensor is based on I2S protocol with dma. My issue is that my project consists of multiple...

FreeRTOS TASK1 stuck while performing continuously communication on UART in TASK2, how to solve this issue?

I created a two task one is for my gsm modem communication through uart and another task is for Bluetooth communication through uart, gam modem communication task is stuck while bluetooth communication task receive data cintinuously.How to resolve t...

JP_RS by Associate II
  • 1180 Views
  • 1 replies
  • 0 kudos

How to set DFSDM Configuration so that LPF cut-off frequency is 1 KHz on MP34DT01-M using STM32F779NI-EVAL?

Hi, I am evaluating MEMS microphone for our application. I am using on board microphone MP34DT01-M in STM32F779NI-EVAL. I am using DFSDM example in STM32F7cube package and able to hear the speech. Now I want to filter the frequencies higher than 1KHz...

The HAL IRQ for HSEM disables itself. Why?

The HAL driver, HAL_HSEM_IRQHandler() disables itself by clearing bits in it's IER register. I don't want it disabled so I have to re-enable it in my HAL_HSEM_FreeCallback(). Is it desirable that it is disabling itself? I'm using the STM32H755.

GHolc.1 by Associate III
  • 964 Views
  • 0 replies
  • 0 kudos

Resolved! File writing bug with FatFs over FreeRTOS on H743

Hi!I would like to store files on an SD card that are transmitted via HTTP POST (lwIP HTTP server). The files are correctly transmitted (hash calculating on both sides, the hashes are equal) and then written out to the card. But the content of the fi...

ranciere by Associate III
  • 2324 Views
  • 4 replies
  • 0 kudos

Resolved! [HAL Bug Report] STM32G474 Cannot use "HAL_ADC_Start_DMA" with ADC5 when ADC3 and ADC4 configured in dual regular mode

Here is the code in question:HAL_StatusTypeDef HAL_ADC_Start_DMA(ADC_HandleTypeDef *hadc, uint32_t *pData, uint32_t Length) { HAL_StatusTypeDef tmp_hal_status; #if defined(ADC_MULTIMODE_SUPPORT) uint32_t tmp_multimode_config = LL_ADC_GetMultimode...

KYin.2 by Associate II
  • 1638 Views
  • 2 replies
  • 0 kudos