STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-F091RC: Zephyr Hello World

Hi, I am trying to get a working demo up for the Zephyr OS on your Nucleo-F091RCbut having trouble. See attached for description, I get this error -"Error: open failedFATAL ERROR: command exited with status 1: /home/jmreina/zephyr-sdk-0.13.0/sysroots...

Justin1 by Senior
  • 2413 Views
  • 1 replies
  • 0 kudos

STM32F427 Ethernet interface with KSZ8081 PHY chip

HiI am using STM32F427 controller. I am using KSZ8081 Ethernet PHY Transceiver.I have configured the controller for MII interface.I have set the IP address and trying to ping the board from PC. There is no response.How to check the controller configu...

PMohan by Associate II
  • 3329 Views
  • 4 replies
  • 0 kudos

AZURE RTOS (ThreadX) with SBSFU WatchDog reset

Hello!I am merging the user app provided in the default sbsfu package with my custom application that is based on the ThreadX kernel. The FW boots normally but every time the kernel finishes ("VOID _tx_initialize_kernel_enter(VOID)") the "tx_applicat...

I am porting a project from stm32f072 to stm32L412 and I am having the link errors listed below. I can't even locate where the symbols are defined.

Error: L6200E: Symbol __asm___18_system_stm32l4xx_c____REV16 multiply defined (by .\system_stm32l4xx_1.o and .\system_stm32l4xx.o).Error: L6200E: Symbol __asm___18_system_stm32l4xx_c____REVSH multiply defined (by .\system_stm32l4xx_1.o and .\system_s...

MKass.1 by Associate II
  • 1446 Views
  • 1 replies
  • 0 kudos