STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! zephyr GPIO irq config

Hi,In the GPIO interrupt configuration, the port information is ignored and only the pin number is used for identification. As a result, pins with the same pin number on different ports cannot be enabled as interrupt sources at the same time. stm32_g...

devin-hu by Associate II
  • 339 Views
  • 1 replies
  • 0 kudos

STM32H5 Bootloader USB Stick mass storage

Hi, I want to start a new project with a STM32H503 (might be), and I read many threat talking about USBX FILEX now on this kind of microcontroller.As it is a bootloader, I do not want to use any RTOS.I use to do bootloader with USB host interface to ...

COSEBE by Senior
  • 585 Views
  • 3 replies
  • 0 kudos

Resolved! Changing the ThreadX timebase to 1ms

Due to more performance requirement, i wanted to change the ThreadX timebase to 1ms. To what i have researched till now i need to make the following #define TX_TIMER_TICKS_PER_SECOND to 1000 which is usually set at 100 which is 10ms. Any idea what el...

data sharing between the cores

Hi,I'm using STM32H7 dual core, where the data has to be shared between the cores, so im having totally 21 variables totally 76 bytes, thought of do it like a structure, so where to place the structure exactly for this data sharing. so, this structur...

Cube/USB/CDC / bulk endpoints overlap?

Hi!EDIT: WARNING! This is no real fix... The bug remains...With STM32Cube_FW_F2_V1.9.0 and CDC's /dev/ttyACM0 I had funny glitches on VoidLinux, when i tried full duplex communication (host<>device):some packets never arrived at the USB hostsome shor...

RRIDDICC by Associate III
  • 436 Views
  • 2 replies
  • 1 kudos