STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST patches for MbedTLS 3.6.5

Hello! Quick question about ST patches for MbedTLS 3.6.5 (stm32-mw-mbedtls).Why was the defined(MBEDTLS_MD_SOME_PSA) added here (in library/md.c)?When MBEDTLS_PSA_CRYPTO_C is defined, the only way to define MBEDTLS_MD_SOME_PSA is to define one of MBE...

Moemen by Associate II
  • 472 Views
  • 3 replies
  • 1 kudos

Resolved! rt-thread project

I created project in stmcube32mx for h5 microcontroller and it works if I manually replace bl main to bl entryin file startup_stm32h563zitx.s.If this manual replacing is a bug or on purpose?Jan

Jan27 by Associate II
  • 1059 Views
  • 10 replies
  • 3 kudos

Resolved! slow data rate with usb cdc on nucleo-h533

Hi All, I'm building an instrument that needs to stream data to a PC at ~4Mbps. People were claiming nearly twice this with USB CDC so I chose the nucleo-h533 board and started with the Ux_Device_CDC_ACM example. I disconnected the USART code and add...

MScha.8 by Associate II
  • 940 Views
  • 11 replies
  • 3 kudos

STM32L471 BFB2 and FB_MODE question.

Hello,I'm trying DUAL BOOT on STM32L471 and having a problem with SYSCFG->MEMRMP FB_MODE bit.I modified Dual Boot Bank Swap Boot Loader Example for STM32G4 project to fit my board, and everything goes well when the firmware put from the start of BANK...