STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

WHY AZURE RTOS Usbx take time to initialize?

Hello,I am working on Nucleo-h745ziq board. According the Ux_Device_CDC_ accordingly I create project for Nucleo-H745ziq board. After connecting the user USB to port I have to go device driver and update the port after that I get the port in Tera ter...

MDeva.1 by Associate II
  • 738 Views
  • 1 replies
  • 0 kudos

Resolved! If I want to use UCPD2 in STM32G0B1RCT6, is HSI16 the only choice as the driving clock for this integrated PD controller? May i use HSE?

In my application, UCPD2 will be active for USB type C PD Sink (45W), which will be working together with other peripherals, such as timers, USB(DEVICE), etc. If the driving clock for UCPD2 is HSI16(in datasheet described), if no other choice, that m...

0693W00000HoVNTQA3.png
Lmatt.11 by Associate III
  • 2568 Views
  • 3 replies
  • 0 kudos

Is there a simple way to use SDMMC1 an fatFS with NucleoH723 (I'm targetting H730 chip) polling or DMA

I try the code bellow an ST youtube video, about F7, sdmmc and fat FS, but it's not working.It seems to me there is no easy way about using SDMMC with H7.the DMA setting are to complicated for my knowledge, but maybe I am missing some point.Is there ...

Tbill.1 by Associate II
  • 1211 Views
  • 2 replies
  • 0 kudos

We found some time the UART interrupt call back function (HAL_UART_RxCpltCallback) will shut down but the IRQ function (UART5_IRQHandler ) still working. Because we have add the counter in call back function and IRQ function 。

We found some time the UART interrupt call back function (HAL_UART_RxCpltCallback) will shut down but the IRQ function (UART5_IRQHandler ) still working. Because we have add the counter in call back function and IRQ function , when the communication ...

User.100 by Associate II
  • 1774 Views
  • 3 replies
  • 0 kudos