2020-12-07 3:34 PM
Hi, this subject has already been treated with other boards in other forums, but libraries and tools have changed since then so i thougth i could open a new question.
So i use CAN1 bus in the Discovery STM32F407 in order to share data between 2 discovery. I use a classic transceiver SN65HVD234 from Texas Instruments. I configured the Discovery with CubeMX and used CubeIDE. I'm using the HAL Library.
I use the User button to fire an EXTI interuption that call HAL_CAN_AddTxMessage() an writes on the bus.
Transmitting data works but not Receiving.
The Hardware is working very well as you can see [in the picture][1]. However the end of the frame bothers me a bit, i don't know if this is nominal.
Here's what I found using the debugger : The interruption enabled for FIFO0 never fires and the function HAL_CAN_RxFifo0MsgPendingCallback() is never called.
So I think the problem comes frome the Filter and its registers that i don't really understand.
here is the configuration code : It does not rise any error handler during the initialization.
CAN_HandleTypeDef hcan1;
/* CAN1 init function */
void MX_CAN1_Init(void)
{
hcan1.Instance = CAN1;
hcan1.Init.Prescaler = 17;
hcan1.Init.Mode = CAN_MODE_NORMAL;
hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan1.Init.TimeSeg1 = CAN_BS1_6TQ;
hcan1.Init.TimeSeg2 = CAN_BS2_3TQ;
hcan1.Init.TimeTriggeredMode = DISABLE;
hcan1.Init.AutoBusOff = DISABLE;
hcan1.Init.AutoWakeUp = DISABLE;
hcan1.Init.AutoRetransmission = DISABLE;
hcan1.Init.ReceiveFifoLocked = DISABLE;
hcan1.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN1_Init */
CAN_FilterTypeDef sFilterConfig;
/*##-2- Configure the CAN Filter ###########################################*/
sFilterConfig.FilterBank = 1;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig.FilterIdHigh = 0x0000;
sFilterConfig.FilterIdLow = 0x0000;
sFilterConfig.FilterMaskIdHigh = 0x0000;
sFilterConfig.FilterMaskIdLow = 0x0000;
sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.SlaveStartFilterBank = 2;
if (HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig) != HAL_OK)
{
/* Filter configuration Error */
Error_Handler();
}
/*##-3- Start the CAN peripheral ###########################################*/
if (HAL_CAN_Start(&hcan1) != HAL_OK)
{
/* Start Error */
Error_Handler();
}
/*##-4- Activate CAN RX notification #######################################*/
if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO1_MSG_PENDING)
!= HAL_OK) {
/* Notification Error */
Error_Handler();
}
if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING)
!= HAL_OK) {
/* Notification Error */
Error_Handler();
}
/*##-5- Configure Transmission process #####################################*/
TxHeader.StdId = 0x321; // 321 MCU1
TxHeader.ExtId = 0x00;
TxHeader.RTR = CAN_RTR_DATA;
TxHeader.IDE = CAN_ID_STD;
TxHeader.DLC = 2;
TxHeader.TransmitGlobalTime = DISABLE;
/* USER CODE END CAN1_Init */
}
void HAL_CAN_MspInit(CAN_HandleTypeDef* canHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(canHandle->Instance==CAN1)
{
/* USER CODE BEGIN CAN1_MspInit 0 */
/* USER CODE END CAN1_MspInit 0 */
/* CAN1 clock enable */
__HAL_RCC_CAN1_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
/**CAN1 GPIO Configuration
PD0 ------> CAN1_RX
PD1 ------> CAN1_TX
*/
GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF9_CAN1;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
/* USER CODE BEGIN CAN1_MspInit 1 */
/* CAN1 interrupt Init */
HAL_NVIC_SetPriority(CAN1_RX0_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(CAN1_RX0_IRQn);
HAL_NVIC_SetPriority(CAN1_RX1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(CAN1_RX1_IRQn);
/* USER CODE END CAN1_MspInit 1 */
}
}I tried to stick to the [STM32F4][2] Ref manual but it didn't work.
[1]: https://i.stack.imgur.com/cm3rp.png
Solved! Go to Solution.
2021-01-05 7:59 AM
Problem Solved !
I did'nt really found why it was not working on my first prototype but I faced the same issue with my final PCB.
However there was a short circuit between the CAN TX and RX on one MCU due to a thin wire of tin !
Even with that problem i had the RX signal on my scope that's why i did'nt thought it was a hard problem !
I removed the bad soldering and modifed the prescalers to have a lower baudrate : 150 Kbits/s .
The design finaly worked with this configuration :
/* Private variables ---------------------------------------------------------*/
CAN_HandleTypeDef hcan1;
/* USER CODE BEGIN PV */
CAN_HandleTypeDef hcan1;
CAN_TxHeaderTypeDef pHeader; //declare a specific header for message transmittions
CAN_RxHeaderTypeDef pRxHeader; //declare header for message reception
uint32_t TxMailbox;
uint8_t a,r; //declare byte to be transmitted //declare a receive byte
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_CAN1_Init(void);
/* Private user code ---------------------------------------------------------*/
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_CAN1_Init();
/* USER CODE BEGIN 2 */
CAN_Config();
a = 0xff;
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_Delay(1000);
//function to add message for transmition
if(HAL_CAN_AddTxMessage(&hcan1, &pHeader, &a, &TxMailbox) != HAL_OK){
Error_Handler();
}
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_2);
HAL_Delay(100);
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_2);
}
/* USER CODE END 3 */
}
/**
* @brief CAN1 Initialization Function
* @param None
* @retval None
*/
static void MX_CAN1_Init(void)
{
/* USER CODE BEGIN CAN1_Init 1 */
/* USER CODE END CAN1_Init 1 */
hcan1.Instance = CAN1;
hcan1.Init.Prescaler = 20;
hcan1.Init.Mode = CAN_MODE_NORMAL;
hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan1.Init.TimeSeg1 = CAN_BS1_12TQ;
hcan1.Init.TimeSeg2 = CAN_BS2_1TQ;
hcan1.Init.TimeTriggeredMode = DISABLE;
hcan1.Init.AutoBusOff = DISABLE;
hcan1.Init.AutoWakeUp = DISABLE;
hcan1.Init.AutoRetransmission = DISABLE;
hcan1.Init.ReceiveFifoLocked = DISABLE;
hcan1.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan1) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief Configures the CAN.
* @param None
* @retval None
*/
static void CAN_Config(void)
{
CAN_FilterTypeDef sFilterConfig;
pHeader.DLC=1; //give message size of 1 byte
pHeader.IDE=CAN_ID_STD; //set identifier to standard
pHeader.RTR=CAN_RTR_DATA; //set data type to remote transmission request?
pHeader.StdId=0x244; //define a standard identifier, used for message identification by filters (switch this for the other microcontroller)
pHeader.ExtId = 0x01;
pHeader.TransmitGlobalTime = DISABLE;
//filter one (stack light blink)
sFilterConfig.FilterFIFOAssignment=CAN_RX_FIFO0; //set fifo assignment
sFilterConfig.FilterIdHigh = 0x0000;
sFilterConfig.FilterIdLow = 0x0000;
sFilterConfig.FilterMaskIdHigh = 0x0000;
sFilterConfig.FilterMaskIdLow = 0x0000;
sFilterConfig.FilterScale=CAN_FILTERSCALE_32BIT; //set filter scale
sFilterConfig.FilterActivation=ENABLE;
sFilterConfig.FilterBank = 0;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.SlaveStartFilterBank = 14;
if (HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig) != HAL_OK)
{
/* Filter configuration Error */
Error_Handler();
}
if (HAL_CAN_Start(&hcan1) != HAL_OK)
{
/* Start Error */
Error_Handler();
}
if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
{
/* Notification Error */
Error_Handler();
}
}
So setting all the filters to 0 permits to accept all CAN messages and it is working.
For those who face the same issue (according to my experience) :
2020-12-16 6:32 AM
I am also facing same issue in case of STM32F107x as well. Transmit is working and Recieve is not working. I tried in Loop back mode as well, but no use.
If you got any update, Please let me know.
2020-12-29 4:53 AM
So we tried with the old library std but it does not work either. We also tried with STM32F405 microcontrolers . We will keep debugging, maybe it has something to do with the baudrate or internal registers ... I would be very happy if someone had experience with this kind of issues !
2021-01-05 7:59 AM
Problem Solved !
I did'nt really found why it was not working on my first prototype but I faced the same issue with my final PCB.
However there was a short circuit between the CAN TX and RX on one MCU due to a thin wire of tin !
Even with that problem i had the RX signal on my scope that's why i did'nt thought it was a hard problem !
I removed the bad soldering and modifed the prescalers to have a lower baudrate : 150 Kbits/s .
The design finaly worked with this configuration :
/* Private variables ---------------------------------------------------------*/
CAN_HandleTypeDef hcan1;
/* USER CODE BEGIN PV */
CAN_HandleTypeDef hcan1;
CAN_TxHeaderTypeDef pHeader; //declare a specific header for message transmittions
CAN_RxHeaderTypeDef pRxHeader; //declare header for message reception
uint32_t TxMailbox;
uint8_t a,r; //declare byte to be transmitted //declare a receive byte
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_CAN1_Init(void);
/* Private user code ---------------------------------------------------------*/
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_CAN1_Init();
/* USER CODE BEGIN 2 */
CAN_Config();
a = 0xff;
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_Delay(1000);
//function to add message for transmition
if(HAL_CAN_AddTxMessage(&hcan1, &pHeader, &a, &TxMailbox) != HAL_OK){
Error_Handler();
}
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_2);
HAL_Delay(100);
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_2);
}
/* USER CODE END 3 */
}
/**
* @brief CAN1 Initialization Function
* @param None
* @retval None
*/
static void MX_CAN1_Init(void)
{
/* USER CODE BEGIN CAN1_Init 1 */
/* USER CODE END CAN1_Init 1 */
hcan1.Instance = CAN1;
hcan1.Init.Prescaler = 20;
hcan1.Init.Mode = CAN_MODE_NORMAL;
hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan1.Init.TimeSeg1 = CAN_BS1_12TQ;
hcan1.Init.TimeSeg2 = CAN_BS2_1TQ;
hcan1.Init.TimeTriggeredMode = DISABLE;
hcan1.Init.AutoBusOff = DISABLE;
hcan1.Init.AutoWakeUp = DISABLE;
hcan1.Init.AutoRetransmission = DISABLE;
hcan1.Init.ReceiveFifoLocked = DISABLE;
hcan1.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan1) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief Configures the CAN.
* @param None
* @retval None
*/
static void CAN_Config(void)
{
CAN_FilterTypeDef sFilterConfig;
pHeader.DLC=1; //give message size of 1 byte
pHeader.IDE=CAN_ID_STD; //set identifier to standard
pHeader.RTR=CAN_RTR_DATA; //set data type to remote transmission request?
pHeader.StdId=0x244; //define a standard identifier, used for message identification by filters (switch this for the other microcontroller)
pHeader.ExtId = 0x01;
pHeader.TransmitGlobalTime = DISABLE;
//filter one (stack light blink)
sFilterConfig.FilterFIFOAssignment=CAN_RX_FIFO0; //set fifo assignment
sFilterConfig.FilterIdHigh = 0x0000;
sFilterConfig.FilterIdLow = 0x0000;
sFilterConfig.FilterMaskIdHigh = 0x0000;
sFilterConfig.FilterMaskIdLow = 0x0000;
sFilterConfig.FilterScale=CAN_FILTERSCALE_32BIT; //set filter scale
sFilterConfig.FilterActivation=ENABLE;
sFilterConfig.FilterBank = 0;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.SlaveStartFilterBank = 14;
if (HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig) != HAL_OK)
{
/* Filter configuration Error */
Error_Handler();
}
if (HAL_CAN_Start(&hcan1) != HAL_OK)
{
/* Start Error */
Error_Handler();
}
if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
{
/* Notification Error */
Error_Handler();
}
}
So setting all the filters to 0 permits to accept all CAN messages and it is working.
For those who face the same issue (according to my experience) :