cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 issue with USB DMA

Gabriel T
Senior

Hi,

I am working with STM32H743ZI

When I enable USB DMA, writing enable here :0693W000006FzgbQAC.png 

I have 3 bytes of offset in my frames, my frame is supposed to start with aa:55:dd:aa instead of 00:00:00:aa:55:dd:aa0693W000006FwU8QAK.pngIt is fixed when I disable DMA but I want to use it

Here is my memory usage :

0693W000006GR8mQAG.pngAny parameter I am missing ?

Regards,

Gabriel

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Ons KOOLI
Senior III

Hi Gabriel,

No, for H7 devices DTCM could not be accessed when enabling DMA USB.

Please refer to this FAQ, it should be helpful. It is wrote for the use of DMA peripheral in STM32H7 devices, but this is applicable when using DMA for USB too.

Best Regards,

Ons.

View solution in original post

5 REPLIES 5
Ons KOOLI
Senior III

Hi Gabriel,

Can you attach your .ioc file as well your linker file?

Best Regards,

Ons.

Gabriel T
Senior

I attached a zipped file with .ioc , flash.ld and ram.ld

Ons KOOLI
Senior III

Hi Gabriel,

Can you please disable the cache when using USB DMA.

Please use a non cacheable memory region.

Best Regards,

Ons.

Gabriel T
Senior

Hi,

If I get it right, I should put buffers used by USB in DTCM RAM but will the USB DMA be able to access it ?

Regards,

Gabriel

Ons KOOLI
Senior III

Hi Gabriel,

No, for H7 devices DTCM could not be accessed when enabling DMA USB.

Please refer to this FAQ, it should be helpful. It is wrote for the use of DMA peripheral in STM32H7 devices, but this is applicable when using DMA for USB too.

Best Regards,

Ons.