STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with adding extra charts to Azure Platform

Recently i imported example to Stm32CubeIDE and in this example i have only one chart. I don't have idea how to add extra charts. if anyone have idea how to add it please tell me or give me some explanations where i need to put or create datas in my ...

DJadc.1 by Associate II
  • 1762 Views
  • 3 replies
  • 0 kudos

Resolved! No response from bootloader after entering

Hello,I am trying to communicate with the bootloader by serial.Most of the times it works nice but sometimes it fails as I fail to enter the bootloader.To give a context, in order to enter the bootloader I set the rts of my FTDI high (this will set t...

0693W00000LyMK2QAN.png
JPatr.3 by Associate II
  • 2529 Views
  • 2 replies
  • 0 kudos

Bootloader on MCU

Hello everyone, i've been coding a bootloader for STM32L072 MCU's, i can download the binary file and write it into FLASH memory from specific address, all this process works, but at the time to jump to the code to be executed, it doesn't work...i ch...

0693W00000LyIBzQAN.jpg 0693W00000LyICdQAN.jpg
RComa.1 by Associate II
  • 2610 Views
  • 4 replies
  • 0 kudos

STM32G4 FDCAN HAL Driver Issue (v1.5.0)

The HAL_FDCAN_ErrorCallback is erroneously being called during every interrupt after a Protocol Error (PEA) occurs, even when no error exists during the interrupt. I believe this condition will occur for some of the other interrupts as well (ELO, WDI...

DAshb.11 by Associate
  • 2509 Views
  • 0 replies
  • 1 kudos

Resolved! What could be causing the STM32L152 UART Rx interrupt to intermittently not fire when data arrives and interrupts are correctly configured?

Hello all,First off, I apologize that I am not able to provide code as everything I have been able to do reproduce this problem is proprietary. Given that, I am looking for advance debugging techniques for diagnosing this intermittent failure of the ...

BCogh.2 by Associate II
  • 3977 Views
  • 5 replies
  • 0 kudos

Resolved! How does Ethernet RX descriptor wrapping work on STM32H7?

My Ethernet driver is not wrapping as I expect.Section "61.10.1 Descriptor Overview" in RM0399 states that descriptors up to N-1 is owned by the DMA and the DMA continues to process descriptors until the Current Descriptor Pointer == Tail Pointer.In...

PWint by Associate III
  • 12464 Views
  • 14 replies
  • 2 kudos