STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Question about frame format of sai

Hi,​I'm implementing signal processing code.(cs42l51 audio in --> stm32 --> cs42l51 audio out)And i'm using STM32H7B3-discovery kit.I have some question about frame format of sai and cs42l51.When i send sine wave data from stm32 to cs42l51, the wavef...

0693W00000LyqwpQAB.png 0693W00000LyqxnQAB.png 0693W00000LyqzKQAR.png
Younjun by Associate III
  • 5266 Views
  • 7 replies
  • 0 kudos

Hard Fault after rewriting part of the flash

Hello there ST Community,I'm currently working in a way to update a device using a USB stick. Instead of implementing a normal bootloader, I decided to try a different approach: have the updater (and all its needed libraries) installed in a fixed reg...

THML by Associate II
  • 2450 Views
  • 5 replies
  • 0 kudos

STM32F407ZG USB DFU Device Descriptor Request Failed

I want to use the factory USB DFU bootloader for production programming. I have set BOOT0 to 1 and BOOT1 to 0, powered on the board, and plugged in the USB, and in device manager I get an unknown device (device descriptor request failed). I am not su...

0693W00000LynsGQAR.png
LLawr.1 by Associate II
  • 1612 Views
  • 1 replies
  • 0 kudos

STSAFEA write/Update with authentication

Hi, I am using STSAFEA to use as a data management (user (32B) + password(32B)). I want to store hash password on the eeprom, but before reading or updating the data I want to do authentication between my MCU and STSAFEA.1.      I was able to send (H...

aabba.1 by Associate III
  • 1380 Views
  • 1 replies
  • 1 kudos

microntroller selection for defence application

I want to build product for defense application. Are there any microcontroller with display capable which is millenary grade certified and has DSP capabilities as well. need 2 SPI and 1 I2C ethernet and serial interface has minimum of 4 MB flash and ...

VPath.1 by Associate
  • 5748 Views
  • 8 replies
  • 0 kudos

STM32H745 USB CDC not working on M4 core

Hi,So with STM32CubeMX is it possible to generate a working CDC (VCP) for the M7 core.I'm unfortunately unable to generate one for the M4 core.What I did (for Nucleo-144):Selected STM32H745ZITxSystem Core->RCC: HSE to bypass mode.Connectivity->USB_OT...

Mvan .31 by Associate II
  • 3030 Views
  • 4 replies
  • 0 kudos