STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 HAL Composite USB Device Example

Posted on November 10, 2014 at 14:30Hello. I am using the new HAL library for writing a program for STM32F4Discovery (for university presentation). The program activates a USB FS CDC device once running to speak with a PC. I've attached an SD card s...

USB MCU not recogniced as a keyboard

Hi! I'm really new to this, so sorry if this is a dumb question, but I'm currently trying to make my STM32nucleo-F103RB work as a keyboard, i've followed a few tutorials but I have a problem when connecting my MCU because when I connect it to my lapt...

jnskf by Associate
  • 3824 Views
  • 1 replies
  • 0 kudos

Resolved! Two definitions forgotten in the STM32F767.svd file

The STM32F767.svd file is provided by the STM32CudeIDE, within the com.st.stm32cube.ide.mcu.productdb.debug_1.5.0.202011051456 directory. The two forgotten definitions are :field CAN3EN in the RCC_APB1ENR register;field CAN3RST in the RCC_APB1RSTR re...

PMoli.1 by Associate
  • 2939 Views
  • 5 replies
  • 1 kudos

USB HID right click button

Hello, I am designing board with stm32f723 with 2 USB. On one side i have mouse attached to STM on other side STM attached to PC. When i transfer report to PC x, y and left click button works fine but i cant make right click. Bellow is the struct of...

IHadz.1 by Associate II
  • 2115 Views
  • 2 replies
  • 0 kudos