STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I need help programming USB FS on Nucleo-F303RE. using pins A11 and A12 and connecting via an exposed USB cable using wires for direct connection to the GPIO's

I believe the programming code might be missing something. I was missing external 1.5K pull up resistors, but I added them and the device is recognized over USB.I would like code references, to implement mass storage mode, with SD card (via SPI).

Resolved! Tasks work strangely in FREERTOS

Started learning FREERTOS and ran into a problem.I showed 3 pieces of code of the same tasks.All 3 pieces of code work differently.Code 1void Task1(void *argument) { int j = 0; for(;;) { HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_0); for(j=0; j<100000...

root437 by Associate II
  • 2823 Views
  • 4 replies
  • 0 kudos

Resolved! Custom bootloader STM32G051

Hi,I want to make custom bootloader on STM32G051. I did something, but it does not work well. After jump to the application it get stucked on some address which correspond HAL_Delay function in my application - it looks like the Systick in my app can...

JR2963 by Senior II
  • 2637 Views
  • 3 replies
  • 1 kudos