Skip to main content
This topic has been closed for replies.
Best answer by Petr Sladecek

Hello,

detailed failure rates for individual functions are provided by ST via specific FMEDA documents. Due to restricted information, these docs are available for customers under NDA exclusively. Please ask your local FAE for support. Current G4 FMEDA includes STM32G473QE data only so you should ask for the doc extension via FAE support anyway. If you are interested at the family general MTBF, it can be expected 469279 years @ 25°C or 38780 years @ 55°C.

Best regards,

Petr

3 replies

NTurr.1
NTurr.1Author
Associate
May 11, 2022

I need Failure rate of STM32g474 for SIL1?

Bob S
Super User
May 11, 2022

Do you mean mean time between failures (MTBF) or failures in time (FIT) values? I think you need to contact your local ST FAE or rep to get those.

Petr Sladecek
Petr SladecekBest answer
ST Employee
May 11, 2022

Hello,

detailed failure rates for individual functions are provided by ST via specific FMEDA documents. Due to restricted information, these docs are available for customers under NDA exclusively. Please ask your local FAE for support. Current G4 FMEDA includes STM32G473QE data only so you should ask for the doc extension via FAE support anyway. If you are interested at the family general MTBF, it can be expected 469279 years @ 25°C or 38780 years @ 55°C.

Best regards,

Petr