STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Query on class b for STM32U585 Controller

Hello Support Team,Have a wonderful day.We are selected Trustzone MCU STM32U585ZIT6Q for our product we have some queries regarding the certification Based on the attached user guide snapshot, we could understand this U5 series chip have a Class B li...

_legacyfs_online_stmicro_images_0693W00000bkRDMQA2.png

Resolved! Hello, Is there an example for the STM32H7 ETH HAL V11.0 (new reworked ETH driver) without the LWIP. All the example i found are coupled with the LWIP. Thanks.

Following function are tied to the LWIP functions and i do not want to use any LWIP etc...How to bypass that ?void HAL_ETH_RxAllocateCallback(uint8_t **buff) { struct pbuf_custom *p = LWIP_MEMPOOL_ALLOC(RX_POOL); if (p) { /* Get the buff fr...

FB__1 by Associate III
  • 2904 Views
  • 2 replies
  • 0 kudos

USB HS MSC ULPI speed optimization

Hi I finaly got my EMMC/SD Card project running. I can read write to my EMMC with ~30 MB/s on a stm32F4. At the moment my USB is too slow. In the forum I read that first thing to do is to multiply MSC_MEDIA_PACKET by 2,4,8, .... THe problem is that a...

MK..1 by Senior
  • 1633 Views
  • 1 replies
  • 0 kudos

Resolved! LwIP RTOS Home Page on NUCLEO-H723ZG not changing

Hi all,I'm trying to create a simple webpage server on a NUCLEO-H723ZG. I understand some basics, but overall I'm pretty new to all of this. So I'm starting from the LwIP Server Netconn RTOS example. If I load the default example to the board, it wor...

Newtham by Associate II
  • 2319 Views
  • 2 replies
  • 0 kudos