cancel
Showing results for 
Search instead for 
Did you mean: 

what's the possible to enter and execute DFU using the nBOOT0 / nSWBOOT0 / OBL_LAUNCH bits information?

bubble
Associate

Hello,

I am using STM32L412RB.

I have some questions about DFU.

STM32L412RB BD is connected to a serial device and receives a specific command.

After that It jumps to the corresponding ADDRESS to perform DFU.

Occasionally, a failure occurs during the DFU process, but re-entry is not possible.

So, I want to know if it is possible to enter and execute DFU using the nBOOT0 / nSWBOOT0 / OBL_LAUNCH bits.

I would like to know what to refer to for related materials.

 Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
MM..1
Chief III