STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-H743ZI ethernet protocol with keil

I want to start the ethernet protocol with NUCLEO-H743ZI. For this I used the following tutorials :https://community.st.com/t5/stm32-mcus/how-to-create-project-for-stm32h7-with-ethernet-and-lwip-stack/ta-p/49308https://github.com/stm32-hotspot/STM32H...

mjadi.1 by Associate
  • 1926 Views
  • 2 replies
  • 0 kudos

DEBUGGER NOT WORKING: STLINK/V2

Hi Team,Recently i was using stm32 stlinkv2 in the STM32F411CEU6. They debugger was workig fine . After flashing 10-20 times , the debugger stopped working and throwig up the error:STMicroelectronics ST-LINK GDB server. Version 7.4.0Copyright (c) 202...

neelimas by Associate II
  • 4916 Views
  • 2 replies
  • 0 kudos

HAL_ADC_Start_DMA did not work stm32g030f6

I encountered the problem that NDM does not work at all on a processor of this model STM32G030F6 ın all versıon cubeidethis is my code /* USER CODE BEGIN Header *//**  ******************************************************************************  * ...

Resolved! PH3-BOOT pin

I did pulled up pin PH3-BOOT high (3.3V). I tried simple code but it looks like it is sitting there and doing nothing. I get this error message. Most chips would have just BOOT pin one function not PH3-BOOT.Multiple errors reported.1) Failed to execu...

0693W00000aJmPBQA0.png
MNapi by Senior III
  • 5578 Views
  • 7 replies
  • 0 kudos

Resolved! STM32C011 Clock Config

Hi @ST Community ,I struggle to configure the clock speed to the frequency I desire.The chip I am using is STM32C011F6U and the code I use as first function in main() is the following:uint16_t cr = RCC->CR;uint16_t cal = RCC->ICSCR;uint16_t cfgr = RC...

saraacri by Associate
  • 2507 Views
  • 2 replies
  • 1 kudos

Reducing the range of BlueNRG-2N

Hello STMicroelectronics community,I'm currently working on a project involving the BlueNRG-2N Bluetooth Low Energy (BLE) module, and I'm looking to reduce the Bluetooth range to approximately 1 or 2 meters (means over 2 meter, I want my bluetooth se...

Walid by Associate
  • 1153 Views
  • 0 replies
  • 0 kudos

About UM2552 sample code

I am building a USBPD sink with reference to the UM2552, but in the sample code on page 16, it seems that the ")" corresponding to the IF on the 9th line has disappeared, is this a typo? Also, is there a correct example somewhere?

Sodag.1 by Associate II
  • 7289 Views
  • 11 replies
  • 0 kudos

Circular buffers and Algobuilder

new to algobuilder.I want to have a float input circular buffer that then goes through an IIR filter. When I add both to algobuilder I can't seem to wire the circular buffer to the IIR filter block, presumably as the circular buffer output bus width ...

Davidcs by Associate
  • 921 Views
  • 0 replies
  • 0 kudos