STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Sensor resolution issue

Hi I am using ISM330DLC sensor and after passing the raw values to the motion_FX library i have got values which are stable but i have found resolution of sensor is varying upto 0.6 how can i improve the resolution of sensor.Thank you!!!

Anil3 by Associate III
  • 1625 Views
  • 2 replies
  • 0 kudos

INTERRUPT problems on custom STM32 F2 board

HI, firstly im new into subject of STM32MCUs. I made my own board based on STM32F2 MCU. I have configured 2 interrupts one based on TIM 11 and one on Button placed at pin 40 (PC9).  It is  simple code including blinking LED every one second and switc...

Zrzut ekranu 2023-11-15 203153.png Zrzut ekranu 2023-11-15 203226.png Zrzut ekranu 2023-11-15 203519.png

STM32H7: DMA+UART+RTS/CTS HW Flow Control

Good evening evryone,I'm actually working on a NUCLEO-H743ZI2 evaluation board and my objective is to develop an mTLS socket via UART.I've configured the UART for working with circular DMA for data reception, and let RTS/CTS works "automatically" (en...

MattiaB by Associate III
  • 2632 Views
  • 2 replies
  • 0 kudos

Resolved! FP-AUD-AEC1 on NUCLEO-F446RE

Hi, I'm trying to get the FP-AUD-AEC1 v1.2.0 acoustic echo cancellation demo application to work.I have a NUCLEO-F446RE board, an X-NUCLEO-CCA02M2 expansion board and an X-NUCLEO-CCA01M1 expansion board.I programmed the NUCLEO-F446RE board with the S...

PascalB by Associate
  • 3358 Views
  • 1 replies
  • 1 kudos

Resolved! STM32H5 MCU package download error

Hi,I cannot download the latest packeges for the H5 MCU-s. From cube IDE I got the error as the attached picture. I got error also from browser from here: https://www.st.com/en/embedded-software/stm32cubeh5.html

MGerz by Associate II
  • 2269 Views
  • 2 replies
  • 0 kudos

Project feasible (DMA-I2S-SPI-SDIO)?

Hi,I was wondering if I can get some feedback on the following project, mainly if the requirements I have are feasible?I was thinking on using an STM32F4 or STM32F7. The project consist of the following parts:An external DAC that is controlled throug...

User10 by Associate II
  • 3023 Views
  • 4 replies
  • 2 kudos

Resolved! STM32L412RB

we're using STM32L412RB microcontroller and it has 2*12 bit ADC and our project requires 8 bit resolution, in this controller can we configure the resolution from 12 to 8 bits?

HTTPS client using STM32F429ZI

Hi,I am attempting to implement HTTPS on STM32 using CubeIDE, but it seems that there are no libraries available for this purpose. Is it possible to achieve this on STM32 using wolfSSL or any other alternative?This is for study purposes; therefore, i...

sonysev by Associate
  • 4554 Views
  • 4 replies
  • 1 kudos