STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FreeRTOS Priority Issue with ETH / LwIP (f746)

I develop a FreeRTOS / LwIP based application which throws a configASSERT error because of a bad priority.Only when the Nucleo is connected to the LAN, the debugger gets stuck at:Line 744 of port.c (FreeRTOS source)configASSERT( ucCurrentPriority >= ...

0693W000008yeQzQAI.png 0693W000008yeR4QAI.png
Mnemocron by Associate III
  • 2906 Views
  • 4 replies
  • 0 kudos

STM32H7 Ethernet With FreeRtos and LWIP

Hello,using the STM32H7 Ethernet with FreeRtos and LWIP results in not sent packages as the Optimization is Turned higher than -O0. The lwip Stack ,for example, tries to send UDP Packages. Those packages never leave the STM32 and UDP data packets ar...

STM32H7 Hal Ethernet Use of LWIP_MEMPOOL_DECLARE

Not sure if this is a bug or something I do not completely understand, but in the generated ethernetif.c file (HAL V1.9.0) there is the line:LWIP_MEMPOOL_DECLARE(RX_POOL, 10, sizeof(struct pbuf_custom), "Zero-copy RX PBUF pool");Which always uses, if...

JRS by Associate III
  • 12888 Views
  • 18 replies
  • 6 kudos

Bug in STM32WBXX_HAL_RTC

As of version 1.12.0, HAL_RTC_Init uses a macro named __HAL_RTC_IS_CALENDAR_INITIALIZED. It is defined as follows:#define __HAL_RTC_IS_CALENDAR_INITIALIZED(__HANDLE__) ((((RTC->ISR) & (RTC_ISR_INITS)) == RTC_ISR_INITS) ? 1U : 0U)I suppose it should r...

LWChris by Associate III
  • 2498 Views
  • 4 replies
  • 0 kudos

Resolved! STM32U5A5 HS Example

Hi guys.Im trying to port an application from STM32F4 over to U5A5.On the F4 i used an external usb hs phy. I was extremely delighted to find out that the new U5 has an integrated hs phy, only to see that:1. No more ST stack in cubemx. Ok, found a gi...

PMera.1 by Associate III
  • 2197 Views
  • 1 replies
  • 0 kudos

[STM32H753] CRYP FIFOs flush for AES

Hello,According to the Reference Manual v8 of STM32H753 one has to to flush the FIFO to perform a cipher operation:  The STM32Cube source code example is not doing this flush for AES-GCM (it does the flush for DES and TDES)I implemented my code like ...

Gpeti_0-1701083358772.png
Gpeti by Senior II
  • 1565 Views
  • 1 replies
  • 0 kudos

ADC_STm32G0

hi..I have tried all the ways to read ADC values as I found that using PA11(ADC_IN15) and PA12(ADC_IN16) is the issue.I tried setting up non configured mode  with polling and also DMA (as per CubeG0 examaples) I couldnt able to read the values. Can a...

meena by Associate III
  • 1272 Views
  • 1 replies
  • 0 kudos