cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo L433RC-P flash program (read/write data)

I want to store some data into flash (read/write)..i have no idea wheter it can be done with Nucleo L433RC-P DK. if possible plz share the example code

i tried with an example code (github - controllerstech F1, F4, H7 series) . but no use of it

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee

Hello @Nagendra A Karmarkar​ and welcome to the Community :)

You can use the available "Flash" example within STM32CubeL4 package:

STM32Cube_FW_L4_V1.17.2\Projects\NUCLEO-L432KC\Examples\FLASH\FLASH_WriteProtection

STM32CubeL4/Projects/NUCLEO-L452RE/Examples/FLASH at master · STMicroelectronics/STM32CubeL4 · GitHub

Hope this helps you!

When your question is answred, please close this thread by choosing Select as Best. This will help other users find that answer faster.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Piranha
Chief II

> i have no idea wheter it can be done

Then try reading the reference manual!