STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

issue with UART call back function

Hello Everyone!!i am using HAL_UART_RxCpltCallback function in my program,  whenever i receive 9 bytes of data via uart an interrupt will trigger and the above mentioned function will get called and execute but  the issue is if i sent a 9 bytes comma...

Anil3 by Associate III
  • 2183 Views
  • 2 replies
  • 0 kudos

STM32F072 CAN LoopBack error on logic analyzer

 Dear reader,I am trying to get the CAN peripheral on my STM32-NUCLEO board working. To start off i wanted to test the loopback mode before I hooked up my transceiver circuit.Heres my init code for the can peripheral generated by CubeMX:Heres my CAN ...

Oli98_1-1701379345715.png Oli98_2-1701379430426.png Oli98_3-1701379475889.png Oli98_4-1701379662680.png
Oli98 by Associate III
  • 1687 Views
  • 2 replies
  • 0 kudos

Unable to set default PHY stm32wb55rg

We're using the stm32wb55rg as the core MCU in a project requiring decently high-frequency BLE notifications to a mobile device (100Hz update rate on the characteristic). In testing this I found that, with default settings, the bluetooth connection w...

Redrield by Associate
  • 2012 Views
  • 1 replies
  • 1 kudos

STM32 RNDIS USB device disappear after a while

Hello,I'm opening a new conversation to address another issue(Issue with VCP and RNDIS ). Previously, I successfully implemented RNDIS on an MCU, and I can see the Remote NDIS based Sharing Interface in the device manager. However, after about 20 sec...

dnj_0-1701342901354.png dnj_1-1701343277723.png dnj_2-1701343651192.png
dnj by Associate III
  • 1744 Views
  • 0 replies
  • 0 kudos