cancel
Showing results for 
Search instead for 
Did you mean: 

AzureRTOS with CubeMX makefile generates IAR files instead of GNU

HDøss.1
Associate II

I'm trying to generate a project using the AzureRTOS software expansion package. When generating code through STM32CubeIDE the correct files are generated (I'm using a GNU ARM compiler), however when I set the Makefile option in CubeMX some files are generated for the IAR system instead of GNU. This causes compilation error. Is there a setting to make sure that the GNU files are generated instead of IAR?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Sara BEN HADJ YAHYA
ST Employee

Hello @Hermund Døssland​, @NRedd.2​,

This issue is fixed in STM32CubeMX latest release.

V6.7.0 is now available under this Link.

Thanks for your contribution :smiling_face_with_smiling_eyes:

Sara.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

8 REPLIES 8
mattias norlander
ST Employee

@Sara BEN HADJ YAHYA​, any idea?

Sara BEN HADJ YAHYA
ST Employee

Hello @Hermund Døssland​ ,

Sorry for the late reply,

Could you please share your ioc file?

thanks,

Sara.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
HDøss.1
Associate II

Hi Sara BEN HADJ YAHYA (Employee),

Here it is, thanks for looking into it!

@Sara BEN HADJ YAHYA​ 

Sara BEN HADJ YAHYA
ST Employee

Hello @Hermund Døssland​ ,

You are right and I confirm the issue, it seems that the IAR folder is generated instead of the GNU folder when a Makefile project is generated.

I've raised this issue internally to be fixed as soon as possible. I'll keep you posted with the updates.

Internal ticket number: 124088 (This is an internal tracking number and is not accessible or usable by customers).

If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly :)

Thanks for your contribution,

Sara.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NRedd.2
Senior

Hi,

This issue still persists in 6.5.0 version.

Could you please fix it?

Hello @NRedd.2​ ,

The dev team is working on this issue, I will let you know once the fix is done.

Sara.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Sara BEN HADJ YAHYA
ST Employee

Hello @Hermund Døssland​, @NRedd.2​,

This issue is fixed in STM32CubeMX latest release.

V6.7.0 is now available under this Link.

Thanks for your contribution :smiling_face_with_smiling_eyes:

Sara.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.