STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Micro SD whith micro controller

Good morning,This is my first postI' m searching for a special micro SD card with:• MCU: 32-bit (produced by ST)• MCU clock: > 100MHz• RAM: > 384 Kbytes• Flash: > 768 Kbytes• Timer function• Random number generator function• Secure memory area requir...

FuscoV by Associate
  • 1679 Views
  • 2 replies
  • 0 kudos

Resolved! STM32G0B1 USB fails to request device descriptor

Hi, I'm running into problems registering USB interfaces on STM32G0B1KBU6.  The same code works fine on STM32F1*, STM32F7*, and STM32G4*.Environment: latest STM32CubeIDE (v.1.13.2) @ Windows.  Target: custom board with STM32G0B1KBU6, which uses the f...

romp by Associate II
  • 2164 Views
  • 1 replies
  • 0 kudos

Resolved! q1.15 Format

I have 1024 integer numbers in an array that are between 0 and 4096. Now I'm trying to convert these array values to Q1.15 format. These should then be between -1 and +1. With my attempt, I don't achieve any negative values, all of them are just posi...

Sax by Associate III
  • 1844 Views
  • 1 replies
  • 1 kudos

Resolved! USB CDC example for STM32F072 (Disco board)

I bought an STM32F072 disco board specifically to develop a USB CDC application, but I can't now find an example or demo in STM32CubeMX V6.10. I found this thread https://community.st.com/t5/stm32-mcus-products/stm32f070-usb-cdc-example/m-p/457994#M1...

Hal_Gettick() always returns 0 for STM32F0 DISCOVERY

Hi, I am working on custom Bootloader and Application stored with different starting address on same Flash When I jump from my Bootloader to Application area which contains Blinking LED With HAL_Delay() function  my application is stuck in HAL_Delay ...

VBAS by Associate
  • 1486 Views
  • 1 replies
  • 0 kudos

Resolved! LT8491

HOW to interface LT8491 BUCK boost converter module  with STM32F103RCt6tr board with i2c protocol and give detailed explanation and if posiible give an example code