STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

About stm32 usb uvc data transmission

sir, Hope you doing all are well.......Presently am working on Stm32f746ZG NUCLEO board. am working on usb uvc communication between MCU and computer.so i need to send image/video data on usb using uvc protocol.I got some developed code from le...

steja by Associate II
  • 3966 Views
  • 2 replies
  • 2 kudos

Any example on STM32F2xx with UVC?

Posted on June 03, 2012 at 13:59Hi, Does anybody know if there is example on STM32F2xx to support UVC class? I checked USB lib provided by STM but only similar example (Audio with ISO out) provided and I do think there should be quite some works if...

USB device with stm32u59

I would like to get started with simple usb device detection and read/write operation , From what i can see , the usb library support is limited to the stm32u5x, my application use freertos but all documentaion i find is regarding USBX and no other u...

Anassoumi by Associate III
  • 956 Views
  • 1 replies
  • 0 kudos

Resolved! FLASH programming issue on HAL_FLASH_Unlock

Hi there!I'm experiencing a new trouble: trying to program a simple flash Word it results in an hard fault; moreover, also trying to read the same area gives an hard fault.Debugging the application I discovered that the HAL_FLASH_Unlock function fail...

iTTy by Senior
  • 3636 Views
  • 2 replies
  • 0 kudos

Resolved! FFT function and buffer size

Watching some videos online about FFT and trying to use (in STM32CubeIDE) the arm_rfft_fast_f32 function of the arm_math.h DSP library, it is not clear to me why the buffer output produced by that function is N/2 long and not NIs it something related...

luke514_0-1706189998758.png
luke514 by Senior
  • 2137 Views
  • 1 replies
  • 1 kudos

ALTCP causes LAN7820 link detection to fail

Working with STM32H743IIT single CM7 core MCU I was managed to have a stable product with Ethernet connectivity. Thanks everybody (@Piranha especially) for your advicesNow I was going to implement secure communication over ALTCP instead of regular ma...

ktrofimo by Senior III
  • 1305 Views
  • 0 replies
  • 0 kudos

Micro SD whith micro controller

Good morning,This is my first postI' m searching for a special micro SD card with:• MCU: 32-bit (produced by ST)• MCU clock: > 100MHz• RAM: > 384 Kbytes• Flash: > 768 Kbytes• Timer function• Random number generator function• Secure memory area requir...

FuscoV by Associate
  • 1679 Views
  • 2 replies
  • 0 kudos

Resolved! STM32G0B1 USB fails to request device descriptor

Hi, I'm running into problems registering USB interfaces on STM32G0B1KBU6.  The same code works fine on STM32F1*, STM32F7*, and STM32G4*.Environment: latest STM32CubeIDE (v.1.13.2) @ Windows.  Target: custom board with STM32G0B1KBU6, which uses the f...

romp by Associate II
  • 2163 Views
  • 1 replies
  • 0 kudos