STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How can b-cams-omv be connected to STM32F746G-DISCO?

Hello,I am trying to connect b-cams-omv(ov5460) camera module into STM32F746G-DISCO board.However I can not find an official sample code examples.I downloaded FP-AI-VISION1_V3.1.0 SW package from ST web-page. When I unzipped it. it found in Drivers\B...

Sejinoh by Associate II
  • 1350 Views
  • 1 replies
  • 0 kudos

Problem with "HAL_UARTEx_ReceiveToIdle_DMA"

Hi,I am using the HAL function "HAL_UARTEx_ReceiveToIdle_DMA" as follows:void HAL_UARTEx_ReceiveToIdle_DMA(UART_HandleTypeDef *huart, uint16_t Size) {//my actionsHAL_UARTEx_ReceiveToIdle_DMA(peripheral, buffer, COMMAND_MAXIMUM_LENGTH);__HAL_DMA_DISAB...

areyzummo by Associate II
  • 4667 Views
  • 7 replies
  • 2 kudos

Ethernet issue after power cycling of STM32H723ZG

I'm having the same problem with STM32H723ZG, with our own board, Ethernet can only be connected after using ST link to download the code (either by "debug" or "run"). After power cycle the board, it won't connect anymore, reset button didn't help.  ...

ETong.1 by Associate II
  • 7998 Views
  • 10 replies
  • 0 kudos

Resolved! STM32H743ZI2 TIMER calculation

Im using stm32h743zi2 microcontroller and , cortext M7 processor , so i need prescalar value and period values of TIM5 for 80milli sec . here im using main clock is 400Mhz and timer bus clock is 200Mhz . please can anyone suggest me a flexible soluti...

STM32L4Q5AGIx Hyperbus PSRAM Issues

We are using a STM32L4Q5AGIx device with Hyperbus PSRAM IS66WVH8M8BLL chip on a custom board.  We are having a number of issues getting the RAM to work corectly on Port 2 and right now are isolating it to reading any of the 4 internal registers, ID0,...

hyperbus_ScopePic.png
BComp by Associate
  • 1411 Views
  • 1 replies
  • 1 kudos