Skip to main content
Kprac.1
Visitor II
Jun 10, 2020 1:13 PM UTC
Question

stm32L072 using bootloader and usb dfu when boot0 is connected to ground

Hi,

I am trying to load the bootloader (on a STM32L072) when my main program is running but after reading a lot of posts talking about this subject it seems that it is not possible to start up the bootloader from the main program due to the dual bank boot management( category 5 devices), after multiples tries, I can't get rid of the bank1 booting.

I can't change my design and boot0 is connected to ground.

Does someone have an idea ?

Thanks,

This topic has been closed for replies.

3 replies

wdaws.1
Visitor II
Mar 18, 2023 7:54 PM UTC

@Kprac.1​ 

wdaws.1
Visitor II
Mar 18, 2023 8:12 PM UTC

@Kprac.1​   Were you ever able to get this to work? I'm trying to do the same.

Tesla DeLorean
Guru
Mar 19, 2023 11:53 AM UTC

I suppose one would need to identify a suitable entry point to the code, or the ​places the tests are done.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..