STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32h743zi WINUSB(HS) ISSUE

I AM USING STM32H743ZI IN USB_HS IN CONTROLLER BUT WHEN I CONNECT USB CABLE TO CPU IN DEVICE MANAGER IT DISPLY winUSB BUT IN zadig software not install the libusb driver it seen the driver not install so how how to solve this problem suggest me 

SITARAM by Associate III
  • 1587 Views
  • 2 replies
  • 0 kudos

stm32h563 Azure Netx Multihome Support

Hello,I have created and executed a TCP server project with Azure NetX library using Ethernet. Additionally, I need multihome support in this project. I want multiple clients to connect to a device with a static IP. Can you assist me with this?Best r...

Eakyo.1 by Associate III
  • 3397 Views
  • 4 replies
  • 0 kudos

Resolved! HS USB MSC as Device --> formatting error on Host

Hi,I am trying to set up a basic HS USB MSC project on a custom board with an STM32F723.The project is based on these tutorials from ST, the only difference is, that I'm using USB HS and not USB FS.https://www.st.com/content/st_com/en/support/learnin...

CObri1_0-1707986829194.png CObri1_1-1707986910415.png CObri1_2-1707986995601.png CObri1_3-1707987560888.png
CObri.1 by Associate III
  • 6829 Views
  • 6 replies
  • 2 kudos

Resolved! USB PD Development Environment

X-NUCLEO-DRP1M1 と NUCLE0-G071RB を持っています。USB 開発には x-cube-tcpp を使用します。ただし、構成ファイル (.ioc) を使用すると、コード生成があることに気付きました。設定ファイル(.ioc)を使用したUSBPD設定ファイル(.ioc)を使用してUSBPD用のソフトウェアを開発することはできますか?サンプルプロジェクトはありますか?

forst by Associate III
  • 2135 Views
  • 2 replies
  • 1 kudos

Resolved! USBC PD TCPM on the STM32U5

Hello,I have an application that uses the TCPM/TCPC architecture, with a STM32U5 acting as the port manager, and the FUSB307B as the port controller. I want to use the USB-PD middleware stack for the policy engine, however, when looking at the availa...

rward by Associate
  • 6605 Views
  • 1 replies
  • 0 kudos

STM32F469 processor internal Bootloader issue

I am having an issue using the STM32F469 processor. Previously using the STM32F407 and STM32F373 I have been able to implement a call to the internal bootloader via address 0x1FFF0000 as suggested in many previous posts. It all works fine and dandy a...

SClar.4 by Associate
  • 2783 Views
  • 5 replies
  • 0 kudos

STM32L4 USB low power stop

Posted on May 20, 2016 at 16:47I am porting an existing design from an F107 to a L4 micro in the hopes that I can push sleep current below 50uA.Currently I have only one barrier to achieving this low power: the USB device peripheral. No matter What ...

kobus by Associate II
  • 9235 Views
  • 16 replies
  • 0 kudos