User Activity

Hi All:We have a project to receive pdm microphone based on the STM32L476RG-Nucleo board.We hope to use the SAI to get PDM M1/M2 data vis PDM decoder.The audio clk is 192KHz and the data size is 16 bits in the system.First we used the cube MX to gene...
Dear ST experts: I am a beginner with ST RTOS. I need your help. We have a project using FW in AMICAM1\UltrasoundFFT based on NUCLEO-STM32L476RG . There two threads in the FW. one is AMICAM1_Thread and another is AMICAM1_Thread. The Ultrasound FFT FW...
Dear All:We have project based on the AMICAM1\UltrasoundFFT project and would like add algorithms in it.There are two major thread in the proect as below.First I use simulation data(different frequency tone) instead of real ADC data to test FFT algor...
Kudos from