STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Boot up STM32L031xx from System Memory

The motive is to upgrade the firmware of STM32L031xx using the system bootloader. I am facing 2 issues majorly.1. For this I need to go to boot mode and boot from system memory as per my understanding. STM32L031K6T6 is follows pattern 2 for which the...

SomaliMajumder_4-1717486888476.png

Resolved! Re: USB HOST cannot parse the last EndPoint

Dear A.Ziru,Apparently I'm having the same problem as you when trying to receive MIDI data from a USB device (in this case it's a guitar multi-effects pedalboard). How did you solve the problem? Where and how did you defined that MIDI class descripto...

moreto by Associate II
  • 4084 Views
  • 6 replies
  • 4 kudos

Resolved! Unable to get DMA transfer complete to trigger

I'm using TIM1 to write a DMA buffer to the built-in LED. I'm trying to get the Transfer Complete callback to trigger. I've tried setting hdma->XferCpltCallback to a function. I suspect there is an interrupt enable flag I need to set and probably cle...

mleo2 by Associate III
  • 3659 Views
  • 4 replies
  • 0 kudos

Resolved! Where are the HAL libraries documented?

I've just spent hours trying to get a DMA to trigger and interrupt when transfer is complete. I was using HAL_DMA_Start() instead of HAL_DMA_Start_IT(). I found HAL_DMA_Start_IT() by looking through the source code.Where are the HAL libraries documen...

mleo2 by Associate III
  • 2282 Views
  • 3 replies
  • 3 kudos

Resolved! NUCLEO-STM32h7s3l8 & USB-HOST

Hello everyone. I recently purchased a Nucleo STM32H7S3L8 board, and it is giving me problems. I am using STM32CUBEIde to create a usb host and a CDC class. I am using the x-cube-tcpp module, USB_OTH_HS and the problem is that the usb host does not i...

Resolved! STM32U5A9 FDCAN Help

I am using a Riverdi STM32 Embedded Display RVT50HQSNWC00-B and having issues with the FDCAN bus. I am capable of writing to the TxFifo and can communicate with an external device in external loop back mode and normal mode. In external and Internal L...

Potential Bug in stm32fxx_STLstartup.c V2.2.0

Dear Community Members, While working on my current STM32F103 project and attempting to integrate the X-CUBE-CLASS-B Library, I've come across a potential issue in the file `stm32fxx_STLstartup.c`. Specifically, it concerns line 351:   351   if (STL_...

WWagner by Associate
  • 1657 Views
  • 1 replies
  • 0 kudos