STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Composite HID+CDC (VCP) with STM32F401

Hi,I would like to create a gamepad that is recognized by the computer (windows), and have the Virtual Com Port (CDC) to send en receive data with the computer. For that, I want to create an USB Composite with HID+CDC. I found an exemple on this webs...

STM32F765 Ethernet LWIP Receive Packet Fail

Hello everyone,Now I am trying to test the Ethernet on our custom board with STM32F765 and MAX24287 via MII mode. Firstly I configure to test the transmit receive raw data with diagnostic loopback mode. From oscilloscope I saw the the data output fro...

MNguy.6 by Associate
  • 2192 Views
  • 2 replies
  • 0 kudos

STM32C031C6T6 : wakeup from shutdown mode

Hello,I'm contacting you regarding a support request concerning the wakeup from shutdown mode of the STM32C031C6T6: The issue we're facing is that __HAL_PWR_GET_FLAG(PWR_FLAG_WUF2) returns True when I power up my STM32, even though I haven't triggere...

ouss_mans by Associate II
  • 3846 Views
  • 7 replies
  • 0 kudos

Resolved! stm32l072 adc multi channel reading problem

I am trying to read multiple ADC channels using the Stm32l072 microcontroller, but in CubeMX, the options for rank assignments, which I normally use to read the channels, are not available. After manually adding these rank assignments to the init fun...

amorftor_0-1719228709034.png
amorftor by Associate II
  • 2477 Views
  • 3 replies
  • 0 kudos