STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Connection through ethernet

Hi, I am trying to create a connection through ethernet with lwip however I stuck at netif down I guess it related with flags which are checking the connection. I am using  STM32H735 board. lwip.c file codes are taken from the github (https://github....

Kuttay by Associate III
  • 2818 Views
  • 5 replies
  • 3 kudos

Personal Project help

I am starting a personal project where I will be designing custom hardware and software for a device that would be be similar to a smartphone. I want it to be able to connect bluetooth, wifi, have speakers and use USB-C(power, data transfer, etc.). I...

Identifying stm32F407 vs stm32F411

Is there any way at all in PC software (Either the ST libraries or things like libUSB) to identify whether a device in DFU/Bootloader mode is an F407 or F411? Everything I can find in the USB properties is identical between the two (Same VID/PID, sam...

FreeRTOS + LWIP + UDP

I'm trying to achieve a UDP communication with STM32H753IIT6 and LAN8720A.I use STM32CubeIDE 1.14.0.According to the ST Ethernet and LwIP  example:   Adam BERLINGER edited on ‎2023-12-07 , I create a project, and change the pin layout according to my...

Hamaos_0-1718185156794.png Hamaos_1-1718185655716.png Hamaos_0-1718186299828.png
Hamaos by Associate
  • 2831 Views
  • 1 replies
  • 0 kudos

x-cube-tcpp in real project

We plan to use STM32G0 mcu with UCPD interface and external TCPP03-M20 protection circuit with single bi-directional power path in our smart power bank with replaceable smart battery and USB-C PD dual role power port application. There will be one US...

Resolved! HAL_SAI_Transmit_IT data

I'm using the NUCLEO board NUH723 to develop a project and I need to understand better how the HAL_SAI_Transmit_IT works. In my code I use the HAL_SAI_Transmit_IT to send data to the SAI1 interface --> 48KHz, stereo,32bit: I have to send two buffer o...

carloV by Associate III
  • 1687 Views
  • 1 replies
  • 0 kudos