STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to Configure x-cube-cellular for lwip?

Hello, I am working on B-U585I-IOT02A board, I have downlaoed the x-cube-cellular expansion pack.It is working with bg-96 cellular modem with USE_SOCKETS_MODEM using freeRTOS.I want to use USE_SOCKETS_LWIP for my B-U585I-IOT02A board how do I configu...

Support with fmc nand flash

Hello,I am running a NAND flash with STM32H7 microcontroller using FMC interface. I have referred to Using the high-density STM32F30xxD/E FMC peripheral to drive external memories datasheet for the programming purpose.While communicating with the dev...

HDesa.1 by Senior
  • 7492 Views
  • 15 replies
  • 2 kudos

STM32H745XIH6 SD Card communication issue

Hello,We are using the  Part#STM32H745XIH6 in our current product and it is going to be use in production.We are very near to release the product but at last we are facing the issue in the SD Card communication and below are the details.At power ON, ...

ABora4_0-1719635965212.png
ABora.4 by Associate III
  • 4251 Views
  • 9 replies
  • 1 kudos

I2S in STMG030F6P6TR

So I am using STMG030F6P6TR to play raw audio stored in SPI flash using PT8211 DAC and LM4890S amplifier. I have stored 8 Bit unsigned mono RAW data in 8000HZ in spi flash, retrieved it and pushed the data into the DAC as follows:void playSong(uint16...

Sh7va_0-1720085241447.png Sh7va_1-1720085297443.png
Sh7va by Associate
  • 807 Views
  • 0 replies
  • 0 kudos

Resolved! OPUS EXAMPLE

i have compiled opus lib on H5. but i can not decode data. this is my init function and works fine.   DecConfigOpus.channels = 2; DecConfigOpus.ms_frame = 20; DecConfigOpus.sample_freq = 48000; uint32_t dec_size = DEC_Opus_getMemorySize(&DecC...

nimaltd by Senior
  • 2019 Views
  • 2 replies
  • 1 kudos

STM32H7A3ZITQ_LQFP144 QSPI Timeout Issue

 Hello,I am using the STM32H7A3ZITQ and have encountered an issue while controlling the MT25QL128ABA1ESESF0IT flash memory during the flash read process. I am operating in QSPI mode. During extended aging evaluations, a 5-second timeout (a busy flag ...

khkim_0-1719807496263.png khkim_1-1719807509696.png khkim_2-1719807523399.png
khkim by Associate II
  • 2592 Views
  • 5 replies
  • 0 kudos