STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G071RB RTC init bug.

Please, answer was anyone trying to use RTC with the G071RB microcontroller? I am powerless now. The code generated by cube does not initialize RTC. I checked the entire initialization procedure if it is consistent with the documentation. Everything ...

wuio by Associate II
  • 12183 Views
  • 12 replies
  • 3 kudos

FatFS on STM32U0XX and external flash

I'm a fresher as a Firmware engineer. I'm currently working on dataloggers. I'm using STM32U083C-DK board which contains STM32U083MCT6 MCU. I've written the code for the basic functionality of the device i.e sleep and wakeup logic using STM32CubeIDE....

RB4020 by Associate II
  • 1369 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F401CCU6 EEPROM Emulation

Hi!!!I am want to implement Emulation of EEPROM for STM32F401CCU6 Controller which is having 256kb of flash memory. but not sure of how exactly that i have to use it. I have downloaded X-CUBE-EEPROM software but in that there is no any project relate...

Anil3 by Associate III
  • 3246 Views
  • 4 replies
  • 2 kudos

How to Configure x-cube-cellular for lwip?

Hello, I am working on B-U585I-IOT02A board, I have downlaoed the x-cube-cellular expansion pack.It is working with bg-96 cellular modem with USE_SOCKETS_MODEM using freeRTOS.I want to use USE_SOCKETS_LWIP for my B-U585I-IOT02A board how do I configu...

Support with fmc nand flash

Hello,I am running a NAND flash with STM32H7 microcontroller using FMC interface. I have referred to Using the high-density STM32F30xxD/E FMC peripheral to drive external memories datasheet for the programming purpose.While communicating with the dev...

HDesa.1 by Senior
  • 7478 Views
  • 15 replies
  • 2 kudos