STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G0B1KEU6 USB

Hello,  I am in an Internship and I got to make communicate a board using a STM32G0B1KEU6 with a PC.The pin PA12 is configured to be USB_DP and the pin PA11 is configured to be USB_DN.I don't know how to configure the others parameters and I haven't ...

nono by Associate
  • 2582 Views
  • 3 replies
  • 0 kudos

QSPI driver for STM32U5G9 under ThreadX

Hi,I would like to know if you have some examples to implement a QSPI driver under ThreadX for a STM32U5G9?  According to my readings, LevelX seems to be appropriate  (I am not sure) because we need to implement some basic functionalities (read, writ...

S_D by Associate
  • 1422 Views
  • 1 replies
  • 0 kudos

Resolved! USB CDC and FreeRTOS

Hiin different posts in forum I read ST's USB library is not thread safe. There are no examples with USB CDC and FreeRTOS.Is that true?Thx 

MK..1 by Senior
  • 2535 Views
  • 4 replies
  • 0 kudos

Resolved! Starting FMAC kills Systick in STM32G431

I have the STM32G431 set up to sample ADC2, send the data to the FMAC and then out to DAC1.  It works fine, I have tested all kinds of filters with it.  However, none of the HAL functions that use SysTick work after I start the FMAC.  I'm using the s...

KDesr.1 by Associate III
  • 2016 Views
  • 2 replies
  • 1 kudos