STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 Ethernet Connection Lost

I am using open source lwip ethernet connection code and I am cehcking wireshark if i lose any connection. TCP ECHO parts are my true outputs but i was wondering if ARP parts means that my connection is lost and I reconnect or is it just checking gat...

Screenshot 2024-07-09 152202.png
Kuttay by Associate III
  • 1335 Views
  • 1 replies
  • 0 kudos

Resolved! X-CUBE-CRYPTOLIB cmox_eddsa_sign HardFault

stm32L476VC + CubeMX + IAR + X-CUBE-CRYPTOLIB STM32CubeExpansion_Crypto_V4.2.0 i copy the example from "NUCLEO-L476RG\Applications\ECC\EDDSA_SignVerify" to my project, cmox_eddsa_sign will cause HardFault:The processor has escalated a configurable-pr...

lll by Associate III
  • 4586 Views
  • 10 replies
  • 2 kudos

Resolved! LWIP_RAND uses newlib rand() and fails

CubeMX generated project defines #define LWIP_RAND() ((u32_t)rand()) which fails with the following call stack...and the following assert textassertion "REENT malloc succeeded" failed: file "/build/gnu-tools-for-stm32_12.3.rel1.20240612-1315/src/newl...

Gustavo_AR_1-1726157473699.png

Resolved! reset an stm32f746 discovery

Hi all, on stm32f746 disco, I'm using the Mbed ide but i have the stmcube installed as wellI've been writing a simple updater app that sits at 0x080e0000 with mixed success  switching to a previous project, the code downloads but on running the board...

andy0105 by Associate
  • 1363 Views
  • 1 replies
  • 1 kudos