User Activity

Hi Team,I've recently cloned https://github.com/STMicroelectronics/STM32CubeL5/tree/master/Projects/STM32L562E-DK/Applications/USB-PD/USB-PD_Consumer_1port , for USB PD project.But when i imported the folder into workspace ,the build option is disabl...
Hi Team,I have STM32L562 EDK with me , and can i make a USB PD application with that alone ?, or should i buy x-nucleo-snk1m1 which has TCPP01 for port protection?Expecting a quick replyThanks in advanceNithin
Hi Team, I want to work on USB PD sink , which board would be suitable?, I'm trying for 28V 5A power. I think the firmware for this specification is not available yet. Even though i want to try on. Would you suggest me any board? Is STM32L562 would b...
Hi Team, I need to build USB PD program on ST32L562, The voltage they are expecting is up to 45V. How to do this?RegardsNithin
Kudos from
Kudos given to