STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Enabling HTTPd breaks the whole project

Hi, I'm playing around with lwIP on my Nucleo-H743ZI and I was able to make ping work, udp/tcp echo and snmp too. But when I enable HTTPd the project doesn't wont do compile I just get a lot of undefined references, I tried to make a new project and ...

abeslic by Associate II
  • 13707 Views
  • 15 replies
  • 10 kudos

interfacing PSRAM using FMC

Hi allI have used CubeMx to create an FMC interface to psram(nonmultiplex) 8-bit data 10-bit addressThe data is valid on the rising edge of the fourth clock To have correct data on the data pins the pointer to write data (psram64) must be a 64-bit po...

dorong_0-1728310439012.png dorong_1-1728310491964.png
dorong by Associate II
  • 1104 Views
  • 0 replies
  • 0 kudos

REST API on STM32F4 with lwIP

Dear all,I am using lwIP over STM32F4 and I would add REST API to my project.I try to understand how to do that, and the only way that I have found is to use CGI. The problem is the reply: I can reply only with a static file present in the SDCARD (th...

LFerr.3 by Associate
  • 2135 Views
  • 1 replies
  • 1 kudos

Error stm32 when use button

Hello everyone, I use the button to hold the Semaphore in this task, when I press the button the Semaphore is released, but the error I get is that the button is not pressed but the Semaphore is automatically releasedplsss help me, thank so much

noname8888_0-1728615678428.png

Home grown OS task function call failures

I am writing my own context switcher. I have a couple LED blink tasks for testing. It works fine when the tasks don't call any functions. Everything is inline. But when I include some function calls in the tasks and I get a context switch while in on...

JoeJoe by Associate II
  • 2041 Views
  • 4 replies
  • 1 kudos