User Activity

Hi all,I am using a STM32H747XIH6 MCU.I developed an application using LwIP library.When I connect my circuit directly to the computer, the application works stably. But when I connect the circuit to the LAN network, the application encounters a hard...
Hello there, I'm writing a STM32 update firmware function (using lwIP ) that accepts a HTTP Post Request to send a new .bin file.Spoiler  After selecting a .bin file to transfer from the PC to the MCU. I use the following line to capture the request:...
Hi all,AbstractWe are developing our product based on STM32H7. We would like to use the HTTP server and Netconn to update the firmware for our product. We consider this method easy to use for customers more than Serial or USB. We have tried looking f...
Kudos given to