STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Configure peripherals after sleep

Hi everyone,During developing applications with STM32l476, using HSI16, I choose STOP1 or STOP2 mode to reduce power consumption , and wake up with RTC Alarm.if (HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, RTC_FORMAT_BCD) != HAL_OK) { Error_Handler(); } ...

path321 by Associate III
  • 1036 Views
  • 1 replies
  • 0 kudos

STM32C031C6 ClassB Example Code

Hi Community,I came a cross with a strange error that I can not understand the reason.As I search the read me file of the example project which is shared by ST.It is written as below.2. load the image into the target3. Execute the code- LED4 toggles ...

Embedded_Class_0-1733854797496.png

Resolved! STM32 UART always times out

Hello,I am testing UART via a loopback test. This shows that the expected data is being sent on TX and received on RX, but the receive function always times out.This post stated to clear the OVR and RXNE flags before calling the receive function, but...