STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Wait on HAL_GetTick not working

Hi everyone,I'm new to STM32CubeIDE and encountering an issue with my code. It seems to halt at the following loop:  while ((HAL_GetTick() - tickstart) < wait) { } I've attached the .ioc file for reference. Can someone help me identify why the pr...

mkothuri by Associate II
  • 1750 Views
  • 1 replies
  • 0 kudos

Resolved! void pointers

I faced with an interesting issue. Here is the code:1. Working: void GameScreenPresenter::activate() { IScreen* scr = &view; scr->Func(); } 2. Doesn't work: void GameScreenPresenter::activate() { void* ptr = &view; IScreen* scr = static_cast<IScreen*...

Wiser1201 by Associate II
  • 1271 Views
  • 1 replies
  • 0 kudos

Resolved! FDCAN Error Counters

Hello,Where can I find documentation on the error counters of the FDCAN_ErrorCountersTypeDef structure? I would be particularly interested in how the incrementation of TxErrorCnt behaves if hfdcan1.Init.AutoRetransmission = ENABLE; (How often does th...

MFrie.7 by Associate III
  • 2052 Views
  • 3 replies
  • 1 kudos

Resolved! stm32h745 eth freertos+tcp freertos + lwip

Hello,I am new to the STM environment and need to test if one M7 core is sufficient for my project. I need to use Ethernet (simple GET, POST, and PATCH requests), an LCD touch panel, and a peripheral that requires EXTI interrupts approximately every ...

RafaelS by Associate III
  • 1820 Views
  • 1 replies
  • 0 kudos

Resolved! Configure peripherals after sleep

Hi everyone,During developing applications with STM32l476, using HSI16, I choose STOP1 or STOP2 mode to reduce power consumption , and wake up with RTC Alarm.if (HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, RTC_FORMAT_BCD) != HAL_OK) { Error_Handler(); } ...

path321 by Associate III
  • 1034 Views
  • 1 replies
  • 0 kudos