STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! NMI Fault without any obvious fault bits set

Hi everyone, I'm currently experiencing a strange crash on a STM32G473 and I'm a bit stumped on how to debug it. First the crash: The system is a STM32G473 running FreeRTOS V10.5.1. I have a simple FDCAN ISR which takes the incoming CAN frames and pu...

turbofish by Associate II
  • 3859 Views
  • 8 replies
  • 3 kudos

Resolved! IP Forwarding

Hello, I have a question about LWIP functionality.I'd like to know if it's possible to redirect a tcp request received on the pppos interface, to a device that is connected onto the ethernet interface and listening on the desired port.Thanks in advan...

RPC by Associate III
  • 1513 Views
  • 2 replies
  • 2 kudos

Azure RTOS NetxDuo mDNS domain set issue

Hello, My issue is related to:-MCU: STM32H733Middleware: Azure RTOSMiddleware Component: NetxDuo (6.2.0)Addon: mDNSI am using Azure RTOS with NetxDuo, I implemented a secure https server in my device and implemented mDNS which was working very well f...

faharintisar_0-1721299474711.png

Resolved! FreeRTOS CMSIS V1 Works but not CMSIS V2

I'm using a NUCLEO STM32F303K8 board attempting to use FreeRTOS, and I have a halting problem when I use CMSIS V2. I found this out by just trying to toggle the built-in LED using HAL using one statically allocated task and observing that the LED onl...

kosh04 by Associate
  • 3856 Views
  • 8 replies
  • 3 kudos

Resolved! H743 SDRAM memory failure

Hello,I'm using a STM32H743 and IS42S32160 SDRAM.  The SDRAM is in bank1, and I followed the instructions on how to setup the external memory from this guide:https://community.st.com/t5/stm32-mcus/how-to-set-up-the-fmc-peripheral-to-interface-with-th...

mattcrc_0-1739856723955.png mattcrc_1-1739856818305.png mattcrc_2-1739856926021.png mattcrc_4-1739857059003.png
matt-crc by Senior III
  • 1196 Views
  • 1 replies
  • 0 kudos

STM32H747 + LwIP reassembly timed out

Hi all, I am using a STM32H747XIH6 MCU. I developed an application using LwIP library. When I connect my circuit directly to the computer, the application works stably. But when I connect the circuit to the LAN network, the application encounters a h...

HHuyn.4 by Associate III
  • 947 Views
  • 0 replies
  • 0 kudos