STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F7 Discovery kit + FMC SDRAM

Hello. I tried to initialize SDRAM (I am using STM32F746 discovery kit), but I try to run it as a separate project just for learning. However I encountered the following problem: when I read data from SDRAM in my case starting from 0xC0000000 address...

baev_al by Associate III
  • 1195 Views
  • 1 replies
  • 0 kudos

Overrun problem with USART2 in STM32H723 MCU

Hello,I'm facing a bizarre issue with USART2 in STM32H7 chip.My H7 is connected to 8 F072 chips via UART. Communication with each chip uses a dedicated UART from 1 to 8.All the data exchanges in both RX and TX work fine during normal operativity of m...

FCamp.1 by Associate III
  • 2432 Views
  • 6 replies
  • 4 kudos

Resolved! CUSTOM BOOTLOADER

  ISSUE: STM32F7 Custom Bootloader - Main Application Not Running After JumpDetails:Bootloader Memory Definition: RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 320K FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 1024K QUADSPI (r) : ORIGIN = 0x90000000, LENGTH...

Can freertos block IWDG?

Hello,I am using freertos configured by STM32CubeMx.The IWDG is activated and configured by STM32CubeMx too.I met an issue in my code but this is not the purpose of this post.Due to this issue the STM32L431 stays blocked indefinitly despite the IWDG ...

mich35 by Associate III
  • 2686 Views
  • 6 replies
  • 0 kudos