STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 SPI and DMA transfer/receive issue

I want to transfer a buffer and receive a buffer of data using a full duplex SPI port with DMA on a STM32H7S3L8H (on the NUCLEO-H7S3L8). My problem is I am not able to modify the transfer buffer and have the modified version sent. I only need to modi...

JBias_0-1743204832297.png JBias_1-1743205158404.png
JBias by Associate III
  • 1722 Views
  • 3 replies
  • 1 kudos

Resolved! HAL UART Issues

Hi, I had to recently work on an application that makes use of the UART, and encountered some issues in the HAL (most recent version provided by CubeMX):1) Hal bug?Drivers/STM32G4xx_HAL_Driver/Src/stm32g4xx_hal_uart.c, Line 3825:3831if (!(IS_LPUART_I...

Resolved! H753ZI - UsbX Device not recognized error

Hi,I'm having an issue implementing USB device composite functionality on my Nucleo-H753ZI board. I've been following the tutorial series at https://community.st.com/t5/stm32-mcus/how-to-implement-the-usb-device-composite-class-in-stm32-using/ta-p/64...

ugurtumer4_2-1743059172157.png ugurtumer4_0-1743059098096.png ugurtumer4_1-1743059126900.png ugurtumer4_3-1743059300672.png

Resolved! Need resources for STM32H563ZI nucleo board

I was recently working on STM32H563ZI nucleo board like connecting peripherals like LTE module, I2C sensors like MPU6050, LCD display, SPI modules like W25Q flash storage, USB  and some analog module like potentiometer. As per normal coding of indivi...

Shubham08 by Associate III
  • 1365 Views
  • 2 replies
  • 1 kudos