STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 custom Bootloader

Dear community,My device is a logger. the configuration is over USB (UART vcp) via a web interface.i'm able to connect it, to configure it and store data correctly.i'm using a stm32L05x (whithout embeded DFU) and ,important, no external reset button....

jlecl.1 by Associate III
  • 3331 Views
  • 8 replies
  • 5 kudos

After STOP2 Mode Wake-Up

STM32L496VET6 – EXTI Not Working After STOP2 Mode Wake-Up1. Part NumberSTM32L496VET6, LQFP100Custom-designed hardware (not a development board)2. EnvironmentIDE: STM32CubeIDE v1.15.0STM32CubeMX: v6.11.0HAL Driver Package: STM32CubeL4 v1.18.0Toolchain...

Chintu by Associate II
  • 868 Views
  • 1 replies
  • 0 kudos

Free-RTOS and mDNS

Hello Community!I'm busy with a project that needs support for mDNS, after a long search i can't find any documentation howto implement mDNS on a Free-RTOS system. The examples provided by ST are not aware of any OS (I Think).Can someone share some i...

JDWBE by Associate III
  • 1832 Views
  • 4 replies
  • 1 kudos

Resolved! problems with the RTC WakeUp.

Moved from the Feedback Forum.The Feeedback Forum is not for product questions.Hi,I'm using Keil platform for programme my STM32 L073RZT6 and I am making it in bare metal. I would like to wake up the STM from any sleep mode using and interruption fro...

Flash with bootloader uart issue stm32f405

Hi,I'm trying to flash overt build in uart bootlader stm32 slave device. Here is my setup :Master STM32F4 with tinyUSBSlave STM32WLE5 device Master and slave are connected together over uart. Master has control of boot0 and reset ligne of slave devic...

SBaro.11 by Associate III
  • 3649 Views
  • 2 replies
  • 0 kudos

Resolved! The NUCLEO-U5A5 example doesn't work.

NUCLEO-U5A5ZJ-QSTM32CubeIDE Version 1.17.0STM32Cube MCU Package for STM32U5 Series 1.7.0 In the call chain from main() -> SystemClock_Config() -> HAL_RCC_OscConfig(), HAL_OK is not being returned.It seems that the HSE configuration is failing. After ...