User Activity

This is my Environment:Microcontroller: STM32H723ZET6LWIP is used. No RTOS used.I am setting a Static IP address in the *.ioc file. I am setting the same IP address in the TCP Raw Socket Echo Server to Bind the socket. Over that I am running the Modb...
I am running a modified TCP Echo Server on the IO Board with STM32H723ZET6 MCU, and LWIP enabled on the Board. No RTOS used. I am sending a continuous sequence of Modbus requests from the ModPoll tool to the Modbus server running on the Board.  But t...
How to set the number of simultaneous connections (backlog) in the Raw Socket Listen API? This is the relevant code snippet: /* start tcp listening for echo_pcb */ tcp_echoserver_pcb = tcp_listen( tcp_echoserver_pcb ); In contrast, the BSD/LWIP Socke...
This is regarding the issue I am currently handling. I am using STM3240G evaluation board to run a Modbus server having a TCP Raw socket-based echo server interface which receives Modbus request packets, sent from ModScan32 tool.                     ...
I’ve created an STM32 project using STM32CubeIDE and enabled LWIP and FreeRTOS. My purpose is to run a basic TCP Server program on the STM3240G-Eval board using BSD sockets, containing two threads. I need to use most of the BSD socket calls such as l...