STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cellular with in-modem IP stack

Hello,I am planning to build a cellular application using EC200 as my modem. I prefer to use in modem stack using AT commands due to memory constraint of my MCU. I have come across X Cube Cellular where it is mentioned this setting can be changed usi...

PSaga.1 by Associate III
  • 698 Views
  • 2 replies
  • 1 kudos

SD card formatting using fileX

Hi, It works, apparently a different microSd card works. however, it is strange that, DATALOG2 could write into the card. May i know how shall i perform sd card format function or what to fill up in the function?   Follow-up of the the topic below: S...

Resolved! "Ux_Host_DualClass" example on STM32N6570-DK

There is no test.txt file in my USB drive after the example is run.The board sends this log**** USB OTG HS Dual_Class Host **** USB Host library started. Starting Application Connect your HID or MSC Device USB Device Enumeration FailureTried to at...

ERROR by Senior
  • 1399 Views
  • 9 replies
  • 3 kudos

Resolved! PWM pattern changed after fixed no of cycles

Hi everyone,I am trying to generate sinewave using PWM mode of microcontroller.I am using Discovery Board having STM32F407 microcontroller. System clock and Timer clock are of 8MhzI am using two timers Timer1 for High Frequency switching (500Hz) and ...

PWM_response.jpg
AHayee by Associate II
  • 945 Views
  • 6 replies
  • 2 kudos

STM32H7S7 USB Webcam driver

Hi,We are currently using STM32H7S7 MCU with display and similar USB C circuit from the developer board.I wanted to connect a Web camera and to be able to display video from the screen.I wanted some help and guidance on where to find the driver?does ...

ropodi17 by Associate II
  • 464 Views
  • 1 replies
  • 0 kudos

issue of ThreadX and FDCAN function

Hello @D.Botelho @mƎALLEm  I had an issue of ThreadX and FDCAN transmit as below. I use the stm32g474 and config a threadx and fdcan with stm32cubemx, so far it works well. but when i add some fdcan transmit code, it comes strangely. the code as belo...

dqsh06 by Senior
  • 1536 Views
  • 11 replies
  • 0 kudos