2024-11-04 3:16 PM
I just started looking at the STM32C071 family as an alternative to the STM32F042 and STM32F072 we currently use. To my disappointment the USB stack for the C071 is a total mess (dozens of files and complete spaghetti) and on top of that it seems to be written by Microsoft. So there is absolutely no way we are going to use that.
Did I miss some other option for the USB device library? This USBX stuff definitely is no option at all.
At first glance it looks like there are no significant differences between the USB hardware of the C0 and F0 if only used as device not host. So I am wondering if I can simply use the F0 libraries (which we have debugged and optimized…) on the C0. Or are there any hidden traps?
Solved! Go to Solution.
2026-03-10 4:17 AM
I finally got to porting the code.
One of the things that were not funny was that ST changed some things between F0 and C0 without actually getting a better result. Also quite some stuff has been slightly renamed without changing the function. It took a lot of searching and replacing but the actual algorithms stay the same.
Since we don't use the host functionality we could simply ignore that part of the registers. At least that was a clean downward compatible expansion of the functionality.
2024-11-04 10:11 PM - edited 2024-11-04 10:14 PM
C0 series USB is basically the same as G0 and not the same as F0. You may adopt the G0 stuff. Or use another, not so versatile solution - hint below. ;)
Also, one of recent articles in Knowledge Base describe the process of implementing classic STM32 USB stack on devices without full support: https://community.st.com/t5/stm32-mcus/how-to-use-stmicroelectronics-classic-usb-device-middleware-with/ta-p/599274
2024-11-05 7:41 AM
Thank you. Most likely I will go with modifying my existing code to fit the C071. It looks like there are not many differences in the hardware, besides the host function that I don't need there seems to be only the pointer register for the buffer descriptor that is missing.
ST libraries are such a mess, I really don't want to debug another USB stack. We need the stuff to work reliably and not look like a pot of overcooked spaghetti especially not if it comes with a load of foul M$ sauce.
2025-01-22 6:16 AM
Hi. Out of curiosity, how did you end up resolving the issue? Did you make it work?
I am affraid I have to do the same, so any advice is appreciated.
None of the 'tutorials' that i found online so far is applicable to C0 family and all the examples by ST include RTOS which is the last thing i need right now.
2025-01-22 6:43 AM
I did not get to it yet. Some other projects have priority. But we will need the C0 for future projects, so I will have to address it soon.
I have zero use for that RTOS. It makes no sense to switch to a controller with more memory and then waste it by using such a bloated system. But maybe we are like the dinosaurs, the last ones who are actually capable of programming efficiently instead of stacking libraries…
2025-01-22 9:22 AM - edited 2025-01-22 11:06 AM
i know, right? i guess st is not that interested in bringing new people to their platform, and the old ones... only the strongest should survive...
anyway, if you are (or anyone ended up in this thread) wonder, the tutorial on using old middleware works for C071 (thanks @gbm for the link)
I still have to do some tests but so far it seems operational. Let me try to attach the working files.
In the USB.zip there is an adapted copy of the https://github.com/STMicroelectronics/stm32-mw-usb-device
according to the tutorial from the link above
and the main.c shows the minimum code required.
becides this, one needs to enable usb interface and enable usb global interrupts.
If someone finds a better way, please dont hesitate to share!
2026-03-10 4:17 AM
I finally got to porting the code.
One of the things that were not funny was that ST changed some things between F0 and C0 without actually getting a better result. Also quite some stuff has been slightly renamed without changing the function. It took a lot of searching and replacing but the actual algorithms stay the same.
Since we don't use the host functionality we could simply ignore that part of the registers. At least that was a clean downward compatible expansion of the functionality.